Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design PS SPI Pmod JE7 Hardware system
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 359 subscribers
  • Views 2541 views
  • Users 0 members are here
Related

PS SPI Pmod JE7 Hardware system

e14 Contributor
e14 Contributor over 12 years ago

Hello everyone,

I'm in the process of interfacing my Avnet CC3000-Pmod Compatible Wi-Fi Adapter to the ZedBoard via the JE7 Pmod header, which is connected to the PS.

At first I thought this should be a simple thing, since creating a hardware system that includes SPI was so simple, but ...

When I try to use the SPI device (via the SpiPs device driver), I am stuck in the XSpiPs_PolledTransfer() function, waiting for the status register flag that indicates the transmission has finished (XSPIPS_IXR_TXOW_MASK). The reason that the flag never comes, is that I read nonsense values from the register (a 0x2 in this case).
Then I added the XSpiPs_SelfTest() function, which failed at the very first register read. So I'm guessing there is something wrong with my hardware design.

I got the Zynq IP setup & configured as follows:

  +--------------------------------+
  |         ZYNQ               DDR +-----> DDR
  |                       FIXED_IO +-----> FIXED_IO
  |                       USBIND_0 +-
-+ TTC0_CLK0_IN         M_AXI_GP0 +-
-+ TTC0_CLK1_IN    TTC0_WAVE0_OUT +-
-+ TTC0_CLK2_IN    TTC0_WAVE1_OUT +-
+-+ M_AXI_GP0_ACLK  TTC0_WAVE2_OUT +-
| |                      FCLK_CLK0 +--+
| |                  FCLK_RESET0_N +- |
| +--------------------------------+  |
+-------------------------------------+

SPI 1: MIO 10 .. 15
SS[1] IO MIO 14
SPI 1 MIO 10 mosi
SPI 1 MIO 11 miso
SPI 1 MIO 12 sclk
SPI 1 MIO 14 ss[1]

The clock is set to ca. 16MHz, which is the maximum the CC3000 can take.

Has anybody had any experience with the CC3000 Adapter, Pmod or SPI on the ZedBoard? I'd be very glad for any help, since I'm pretty much stuck here.

With best regards,
Darius

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi, i'm a coworker of Darius. He is currently working on another project and i got assigned to work on the CC3K. I just stumbled over this thread and thought i give you a little heads-up what's been happening in the last months.

    In short: yes, we could solve our problems with the SPI, but not without swapping parts out.

    Long version:
    First try to fix the SPI was to pull the SPI_SS_I signal to high in the top-level HDL-file (because Vivado doesn't have this MHS anymore). With that we didn't experience any resets on the SPI anymore. After that we had the problem that apparently the Zynq-SPI could not handle the delays dictated by the CC3K first-write-sequence while the slave select is active the whole time. To fix this, we abandonned using the slave select of the SPI-Core and used GPIO instead as slave select. When we did this we were finally able to send commands to the CC3K via SPI, but ran into the next problem almost imediately: when the CC3K answers to the commands, we could see the correct answers going over the SPI wires but the RX FIFO of the SPI core contained just 0xFF, over and over again. That was the point where we decided to ditch the Zynq SPI and started using the AXI-SPI IP core from Xilinx. At the beginning this core gave us some troubles too, like not being able to provide a stable SPI clock, but we could fix that by changing the ref_clk settings (we now use a ~32 MHz ref clk for the core and that gives us a ~16MHz SPI clk). With the AXI-SPI and the GPIOs (for en, irq and ss) we were finally able to correctly communicate with the CC3K via SPI.

    Current status:
    Right now, bind(), listen(), accept() and recv() work and we're able to use the ZedBoard as a server. But we still can't use the ZedBoard as a client because connect() does not work. At the moment, we're trying to figure out what goes wrong there. We're using our own drivers, not the ones provided by TI, so maybe we still have a bug in there somewhere. But trying to use the CC3K with an LX9 board and the reference design by avnet (including the drivers by TI) resulted in the same situation: we were able to use it as a server but not as a client because connect() never returned. Any suggestions to fix this would be appreciated.

    Well, that's it up to this point, hope i could help you out a little!

    Best regards,
    Max

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi, i'm a coworker of Darius. He is currently working on another project and i got assigned to work on the CC3K. I just stumbled over this thread and thought i give you a little heads-up what's been happening in the last months.

    In short: yes, we could solve our problems with the SPI, but not without swapping parts out.

    Long version:
    First try to fix the SPI was to pull the SPI_SS_I signal to high in the top-level HDL-file (because Vivado doesn't have this MHS anymore). With that we didn't experience any resets on the SPI anymore. After that we had the problem that apparently the Zynq-SPI could not handle the delays dictated by the CC3K first-write-sequence while the slave select is active the whole time. To fix this, we abandonned using the slave select of the SPI-Core and used GPIO instead as slave select. When we did this we were finally able to send commands to the CC3K via SPI, but ran into the next problem almost imediately: when the CC3K answers to the commands, we could see the correct answers going over the SPI wires but the RX FIFO of the SPI core contained just 0xFF, over and over again. That was the point where we decided to ditch the Zynq SPI and started using the AXI-SPI IP core from Xilinx. At the beginning this core gave us some troubles too, like not being able to provide a stable SPI clock, but we could fix that by changing the ref_clk settings (we now use a ~32 MHz ref clk for the core and that gives us a ~16MHz SPI clk). With the AXI-SPI and the GPIOs (for en, irq and ss) we were finally able to correctly communicate with the CC3K via SPI.

    Current status:
    Right now, bind(), listen(), accept() and recv() work and we're able to use the ZedBoard as a server. But we still can't use the ZedBoard as a client because connect() does not work. At the moment, we're trying to figure out what goes wrong there. We're using our own drivers, not the ones provided by TI, so maybe we still have a bug in there somewhere. But trying to use the CC3K with an LX9 board and the reference design by avnet (including the drivers by TI) resulted in the same situation: we were able to use it as a server but not as a client because connect() never returned. Any suggestions to fix this would be appreciated.

    Well, that's it up to this point, hope i could help you out a little!

    Best regards,
    Max