Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design NEED: Complete Instructions To Use XADC Header
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 361 subscribers
  • Views 1499 views
  • Users 0 members are here
Related

NEED: Complete Instructions To Use XADC Header

e14 Contributor
e14 Contributor over 13 years ago

So we have 3 differential channels to use with this XADC header:

VP/VN,
VAUX0P/VAUX0N
VAUX8P/VAUX8N

I'm sampling at 1 KHz so timing is not an issue for me with the internal mux setup of the XADC.

I see that the requirement for the XADC inputs is a 1V peak-to-peak differential. What is the common-mode voltage? Is it vref (1.25 V)?

What ports do I have to provide other than the differential data lines? Which of the following are already provided for by the board (ie. which are driven out from the XADC header?):

Vref
VCCADC
AGND

How many of our Zedboard brethren have started to do designs that require external sensors and ADCs anyhow? What are your experiences with the XADC header? I didn't find the HW manual itself to be too helpful, and the only "tutorial" uses the onboard thermal sensor. Obviously this is insufficient for applications relying on external sensors.

Thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Is there a way to just input a voltage and read it through the terminal using the XADC Header on the Zynq 7000 Zedboard? If so can this be done using the VP VN pins?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Is there a way to just input a voltage and read it through the terminal using the XADC Header on the Zynq 7000 Zedboard? If so can this be done using the VP VN pins?