Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design I2C PMOD device --> TCP/IP (Ethernet) using Linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 568 views
  • Users 0 members are here
Related

I2C PMOD device --> TCP/IP (Ethernet) using Linux

Former Member
Former Member over 12 years ago

I would like to read data from an i2c device through the PMOD (such as Digilent temp sens) and write to e/net.  I've read the standard Linux OS distributed for the Zedboard has the TCP/IP functionality built in, so I think it's best to just try and use that OS but I need to add the i2c interface. I have a couple questions:

1) How might I add the i2c interface so it is accessible from Linux?
2) How do I actually read info from that device (do i2c devices have addresses for registers typically, and how to access them from Linux?)
3) How does the tcp/ip comms work on Linux?  for instance, I think the standard IP address is 192.168.1.10 for the zedboard, but how to establish a connection with it from my PC to send and receive data?

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    I know the zedboard has SPI1 and I2C1 directly routed to the CPU and SPI1 pins are located to the PMODA. Don't know for the I2C1 pins tho..

    you can also invoke a Xilinx I2c ip (low freq IP catalog)
    which will plug onto the AXi bus and you can access it in baremetal or linux rather fastly (no axi understanding needed)


    you can finally code your personnal IP which you plug onto the axi bus on a specific axi protocol.

    Ethernet is routed to the CPU, don't know much about the ethernet in the Linux kernel but you might access it easily if your linux distribution supports ethernet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    I know the zedboard has SPI1 and I2C1 directly routed to the CPU and SPI1 pins are located to the PMODA. Don't know for the I2C1 pins tho..

    you can also invoke a Xilinx I2c ip (low freq IP catalog)
    which will plug onto the AXi bus and you can access it in baremetal or linux rather fastly (no axi understanding needed)


    you can finally code your personnal IP which you plug onto the axi bus on a specific axi protocol.

    Ethernet is routed to the CPU, don't know much about the ethernet in the Linux kernel but you might access it easily if your linux distribution supports ethernet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data