Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Vectors in Vivados Block Diagram
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 358 subscribers
  • Views 352 views
  • Users 0 members are here
Related

Vectors in Vivados Block Diagram

e14 Contributor
e14 Contributor over 10 years ago

Hi,

I designed a simple proof-of-concept IP core, which I want to connect to the Processing System using the EMIO GPIO.

The IP-Core has only two inputs.
A clock input and a reset input.
These two are two different Ports!
I configured the PS EMIO GPIO to be 2-Bit wide.

Now the problem:
I am not able to figure out how to connect the IP-Core to the PSs EMIO GPIO.
It is not possible to "expand" the GPIO Output Vector of the PS.
How do I get the connection right?
I tried to connect both clk and reset to the GPIO_O pin.
After that I looked at the Verilog file of the Block Diagram and found that both, clk and rst where connected to the [0]'s position of the GPIO_O.

It would be easy to modify this file and fix this but unfortunately, this file is read-only!

As a hotfix, I changed the two separate inputs of the IP-Cote to one 2-Bit Vector, but that can't be the solution..

Is there a better way to do this?

Thanks

  • Sign in to reply
  • Cancel
  • drozwood90
    0 drozwood90 over 10 years ago

    Why don't use use the AXI to connect?  That is the purpose of that interconnect.

    --Dan