Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Scu Timer run at very low Frequency
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 432 views
  • Users 0 members are here
Related

Scu Timer run at very low Frequency

fayyazrafiq
fayyazrafiq over 12 years ago

I am using scu timer and I have some problem with its frequency. As mentioned in  the ug585- page 193.

"Each Cortex-A9 processor has its own private 32-bit timer. These timers are always clocked at 1/2 of the CPU frequency
(CPU_3x2x)."

According to this statement, if my core frequency is 667 MHz, then the timer should run at 667/2. In order to check the timer frequency, I setup scu interrupt and GPIO. After every time out value, I toggle the gpio pin in order to see the frequency. I tried many values, and every time, I found a different frequency. In addition, frequency is around 1.20MHz to 1.35 MHz which is very slower than expected. According to above mentioned, frequency should be half of the core frequency (667/2=333.33 MHz). Can anybody tell me, what is the reason? Am I missing something. Any help is highly appreciated

Regards
Fayyaz

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    I've noticed a slowness problem that might be related to the problem fayyazrafiq is having. I've written a byte-parser (like an XML parser) that takes 4.0 uS on my old Linus web server. It takes 48 seconds under Linux on the Zedboard! Any thoughts?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    I've noticed a slowness problem that might be related to the problem fayyazrafiq is having. I've written a byte-parser (like an XML parser) that takes 4.0 uS on my old Linus web server. It takes 48 seconds under Linux on the Zedboard! Any thoughts?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data