Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design ZedBoard hangs after adding GPIO device
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 358 subscribers
  • Views 133 views
  • Users 0 members are here
Related

ZedBoard hangs after adding GPIO device

Former Member
Former Member over 11 years ago

I've found several topics about the zedboard that hangs at

Starting kernel ...
Uncompressing Linux... done, booting the kernel.

but none of them would give me a solution. When I load my zedboard via TFTP into QSPI with the folowing files, linux hangs.

Files:
- boot.bin (consists of fsbl.elf and u-boot.elf)
- devicetree.dtb
- uImage
- uramdisk.image.gz


all sources are build from scrach.

When I add an GPIO device to the devicetree with the following code the kernel hangs

GPIO code:

   [code]
   axi_gpio_0: gpio@41200000 {
ttt   #gpio-cells = <2>;
ttt   compatible = "xlnx,xps-gpio-1.00.a";
ttt   gpio-controller ;
ttt   reg = <0x41200000 0x10000>;
ttt   xlnx,all-inputs = <0x0>;
ttt   xlnx,all-inputs-2 = <0x0>;
ttt   xlnx,all-outputs = <0x1>;
ttt   xlnx,all-outputs-2 = <0x0>;
ttt   xlnx,dout-default = <0x00000000>;
ttt   xlnx,dout-default-2 = <0x00000000>;
ttt   xlnx,gpio-width = <0x20>;
ttt   xlnx,gpio2-width = <0x20>;
ttt   xlnx,interrupt-present = <0x0>;
ttt   xlnx,is-dual = <0x0>;
ttt   xlnx,tri-default = <0xFFFFFFFF>;
ttt   xlnx,tri-default-2 = <0xFFFFFFFF>;
tt   } ;
   [/code]

when I remove this code from the devicetree.dtb linux runs fine.

How can I solve my problem and let the kernel boot normal?