Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design HDMI Display Controller Tutorial Issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 353 subscribers
  • Views 383 views
  • Users 0 members are here
Related

HDMI Display Controller Tutorial Issue

Former Member
Former Member over 11 years ago

Hello,

I am using the following tutorial to build a vdma based video project.

http://community.em.avnet.com/t5/FMC-HDMI-I-O-VITA-Image-Sensor/FMC-IMAGEON-IP-Cores-and-Tutorials-for-Vivado-2013-3/td-p/8356

I have build the Display controller and everything builds correctly in Vivado 2013.4.  But nothing gets displayed on the monitor.

Can anyone please point out what might be wrong?

(other tutorial examples, passthrough, worked like a charm)

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Take a look at this post for a possible answer:

     

    http://zedboard.org/content/problem-hdmi-interfacing-zedboard

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • albertabeef
    0 albertabeef over 11 years ago

    Hello,
    One common mistake with this tutorial is to expect the color bars on the ZedBoard's HDMI connector.  Can you please confirm that you have your monitor connected to the FMC-IMAGEON module's HDMI output connector ?
    Can you confirm that your monitor supports 1080P60 resolution ?
    Regards,
    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to albertabeef

    Hi Mario,

    Thanks for the quick response.  Yes, I did connect it to the fmc card's HDMI output.  Also the monitor does support 1080P60 resolution.  I think the HDMI passthrough demo is also built for the same resolution, and that has no issues running on this monitor.

    My end goal is to merge these two demos and have HDMI in, VDMA and DDR thing, and then HDMI out. But struggling to get the second demo working :(

    Thanks for all the support 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    I found my solution.  In the tutorial, it assumes reset for High performance bus would be connected automatically to reset of fclk1 but I had to derive freset1 in ARM manually and connect that to the reset system for HP bus

    Thanks for the great reference design!