Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design designing without the ARM prcessor
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 249 views
  • Users 0 members are here
Related

designing without the ARM prcessor

Former Member
Former Member over 13 years ago

Hi All

I know , it would sound weird but I wish to implement a design wherein I do not use the hard core processor. I need to design the system using EDK and microblaze as the processor.Has anyone tried something like this?

Would I need to create a blank XPS Project for this and add the necessary peripherals?

Also , for cascaded JTAG , I am unable to see anything on the hyper terminal. Also in SDK , I am not able to execute and see the output on the virtual hyper terminal, which is selected same as the virtual com port(USB-UART), I do not see anything on the hyper terminal and the LEDs too do not blink.Where could I be going wrong ?




  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 13 years ago

    Haven't tried this yet, but Xilinx recently published this app note:

    Zynq-7000 Example Design - Use of MicroBlaze to output "Hello World" using the PS UART
    http://www.xilinx.com/support/answers/50869.htm

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer