Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design standalone xgpio app freeze on zedboard if I dont boot linux once before...
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 748 views
  • Users 0 members are here
Related

standalone xgpio app freeze on zedboard if I dont boot linux once before...

e14 Contributor
e14 Contributor over 12 years ago

Hi team !

I use a Zedboard rev D
SD linux demo is okay (write_led ...)

I use vivado/xsdk 14.1 (but the same with 13.4)
I have written a test design with dual axi-gpio (v4) and exported to xsdk. everything ok

I boot linux (sw 4-1 ON), then flash (with xsdk) wrapper_system.bit then with xmd :

connect arm hw
source ps7_init.tcl
ps7_init
dow mydemo.elf
con

all leds are happily blinking


BUT the same app, without booting linux first, freeze during XGpio_SetDataDirection

I have reproduce this
I double check design ...

any ideas ?

test app :
int status=XGpio_Initialize(&gpio,XPAR_PS7_GPIO_0_DEVICE_ID);
    if (status != XST_SUCCESS)xil_printf("xgpio_initialize error
r");
    xil_printf("1
r");
    XGpio_SetDataDirection(&gpio,1,0x00);
    xil_printf("2
r");
    XGpio_SetDataDirection(&gpio,2,0x1);
    xil_printf("3
r");
XGpioPs_Config *cfg=XGpioPs_LookupConfig(XPAR_PS7_GPIO_0_DEVICE_ID);
    xil_printf("11
r");
    XGpioPs_CfgInitialize(&gpiops,cfg,cfg->BaseAddr);
    xil_printf("12
r");
    XGpioPs_SetDirectionPin(&gpiops,7,1);
    xil_printf("13
r");

    while (1) {
               xil_printf("on %x
r",XGpio_DiscreteRead(&gpio,2));
               XGpio_DiscreteWrite(&gpio,1,0xaa);
               XGpioPs_WritePin(&gpiops,7,1);
               getchar();
               xil_printf("OFF
r");
               XGpio_DiscreteWrite(&gpio,1,0x55);
               XGpioPs_WritePin(&gpiops,7,0);
               getchar();
           }

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The Rev D ZedBoard has production version of the Zynq device. The BootROM in the production device operates differently than the pre-production or 'ES' silicon and does not bring the PL out of reset after the bitstream is loaded. The production Zynq device was not supported in the Xilinx tools until ISE/SDK 14.2, so you will need to use a newer version of the tools. See this Xilinx Answer Record:

     

    http://www.xilinx.com/support/answers/51807.htm

     

    I would suggest using the Vivado tool suite or, if you want to stay with the PlanAhead/ISE flow, updating to 14.7. The software voucher that came with your ZedBoard should still be valid for software updates.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor


    use of ps7_post_config solve the issue :

    follow rules below :

    connect arm hw
    ps7_init
    flash fpga with wrapper.bit
    ps7_post_config
    dow f.elf
    con