Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design how to communicate with DDR3 in PS on zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 358 subscribers
  • Views 580 views
  • Users 0 members are here
Related

how to communicate with DDR3 in PS on zedboard

e14 Contributor
e14 Contributor over 12 years ago

    hi,I'm a beginner of zedboard, and i am finishing my task to build a video transport system.  and now i have used VDMA to generate the transportation channels( s2mm and mm2s), but i am just troubled about how to communicate with DDR3 on my project.
should I use AXI Interconnect ip core? and has  the master AXI4 port of it been connected to the PS(or DDR3)?  if not, how can i constrain my outputs to finish this communication?
  hurrily wish your reply.

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 12 years ago

    Hi,
    The easiest way to get your video data into the DDR3 is to use the AXI VDMA block.  It seems that you are using that without the AXI interconnect?
    Since your trouble is on the Processor side, there is a video reference design that I think can help you on the Reference Designs/Tutorials page located here:
    http://zedboard.org/design/1521/11
    "FMC-IMAGEON IP Cores and Tutorials for Vivado"

    That tutorial has a solutions file where the VDMA is being used.

    On the PS side, it should be as easy as either reading the memory directly, or less costly in processor cycles - use the DMA.  This will require some work to setup in the software.

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • drozwood90
    0 drozwood90 over 12 years ago

    Hi,
    The easiest way to get your video data into the DDR3 is to use the AXI VDMA block.  It seems that you are using that without the AXI interconnect?
    Since your trouble is on the Processor side, there is a video reference design that I think can help you on the Reference Designs/Tutorials page located here:
    http://zedboard.org/design/1521/11
    "FMC-IMAGEON IP Cores and Tutorials for Vivado"

    That tutorial has a solutions file where the VDMA is being used.

    On the PS side, it should be as easy as either reading the memory directly, or less costly in processor cycles - use the DMA.  This will require some work to setup in the software.

    --Dan