Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard TANGO Control System Gateway
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 362 subscribers
  • Views 748 views
  • Users 0 members are here
Related

Zedboard TANGO Control System Gateway

e14 Contributor
e14 Contributor over 11 years ago

accessing ZedBoard PL from TANGO distributed control system

youtube video https://youtu.be/fH60xha-u6o


paper here : https://docs.google.com/document/d/1HOfuCSrw6B209dEPM7wvXpxm8jWtyQ9mt2t3AShQnJI


Download a ready to launch TangoBox (64 bit OS / VirtualBox required, 1.4GB)
http://dl.free.fr/dWfRMq6Xe
flash zedboard qspi memory with BOOT.bin
http://dl.free.fr/b5O2C4K43

see www.tango-controls.org for more info on TANGO Control system and www.esrf.eu where it was designed and used since 1996.

Tango is a free, open source, distributed, scalable, efficient SCADA framework : a set of tools and API to monitor industrial appliance of any kinds...
Tango control system was elaborated at the ESRF, a large synchrotron radiation facility in Grenoble, France. The ESRF is a large research laboratory (1500 engineers, researchers, ), a kind of giant microscope to explore organic molecules or others and that uses X rays of high energy (6 GeV) issued from an 850 meters circumference accelerator in more than 40 beams lines operating simultaneously. see www.esrf.eu for info.

Tango Control System is a 100 man/years middleware, which aims at the monitoring 24/7 of more than 200 000 sensors & actuators in the facility. It features among other usage : logging, events driven communication, seamless integration to NI Labview, Matlab, Igor scientific toolboxes or OPC-UA plc, EPICS bus, ...

The SKA Telescope (square kilometre array telescope in southAfrica/Australia) will use TANGO. (skatelescope.org)
But Tango can also fit in a raspberry pi or in a zynq SoC ! But it is a serious game...

we enroll in XUP OpenHardware 2015 Contest with this proof of concept.
thank you for reading

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Dear all,

    we registered again a team from the class "Lpro Systèmes embarqués" UJF Grenoble in the Xilinx University Contest, OpenHardware 2016 (http://www.openhw.eu/)


    This app is running on zedboard an use Assymetric Multiprocessor : one ARM core for linux/tango device server and the other one for a standalone bare metal app (human safety can't rely on a non deterministic linux app). Communication use OnChipMemory. Linux is custom OpenEmbedded. We use Zynq internal XADC to monitor the current in Transfer Line between Booster and Storage Ring, this current is an image of the radiation dose.

     

    Tango Distributed Control System : www.tango-controls.org
    ESRF : www.esrf.eu

     

    try it ! download files : 
    zedboard SD : http://dl.free.fr/huOxTADZV
    virtualbox tango/ubuntu image : http://www.tango-controls.org/downloads/virtual-machine/

    document url : https://docs.google.com/document/d/1glvFaKJogfreaWkISOiwTDw1JLJJtfZDZQDQ5kmIFsI


    Youtube here...

    paper here :
    https://docs.google.com/document/d/1glvFaKJogfreaWkISOiwTDw1JLJJtfZDZQDQ5kmIFsI

     

     

     

    Tango is a free, open source, scalable, efficient SCADA framework : a set of tools and API to monitor industrial appliance of any kinds... 
    Tango control system was elaborated at the ESRF, a large synchrotron radiation facility in Grenoble, France. The ESRF is a large research laboratory (1500 engineers, researchers, ), a kind of giant microscope to explore organic molecules or others and that uses X rays of high energy (6 GeV) issued from an 850 meters circumference accelerator in more than 40 beams lines operating simultaneously.

    Tango Control System is a 100 man/years middleware, which aims at the monitoring 24/7 of more than 200 000 sensors & actuators in the facility. It features among other usage : logging, events driven communication, seamless integration to NI Labview, Matlab, Igor scientific toolboxes or OPC-UA plc, EPICS bus, ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Dear all,

    we registered again a team from the class "Lpro Systèmes embarqués" UJF Grenoble in the Xilinx University Contest, OpenHardware 2016 (http://www.openhw.eu/)


    This app is running on zedboard an use Assymetric Multiprocessor : one ARM core for linux/tango device server and the other one for a standalone bare metal app (human safety can't rely on a non deterministic linux app). Communication use OnChipMemory. Linux is custom OpenEmbedded. We use Zynq internal XADC to monitor the current in Transfer Line between Booster and Storage Ring, this current is an image of the radiation dose.

     

    Tango Distributed Control System : www.tango-controls.org
    ESRF : www.esrf.eu

     

    try it ! download files : 
    zedboard SD : http://dl.free.fr/huOxTADZV
    virtualbox tango/ubuntu image : http://www.tango-controls.org/downloads/virtual-machine/

    document url : https://docs.google.com/document/d/1glvFaKJogfreaWkISOiwTDw1JLJJtfZDZQDQ5kmIFsI


    Youtube here...

    paper here :
    https://docs.google.com/document/d/1glvFaKJogfreaWkISOiwTDw1JLJJtfZDZQDQ5kmIFsI

     

     

     

    Tango is a free, open source, scalable, efficient SCADA framework : a set of tools and API to monitor industrial appliance of any kinds... 
    Tango control system was elaborated at the ESRF, a large synchrotron radiation facility in Grenoble, France. The ESRF is a large research laboratory (1500 engineers, researchers, ), a kind of giant microscope to explore organic molecules or others and that uses X rays of high energy (6 GeV) issued from an 850 meters circumference accelerator in more than 40 beams lines operating simultaneously.

    Tango Control System is a 100 man/years middleware, which aims at the monitoring 24/7 of more than 200 000 sensors & actuators in the facility. It features among other usage : logging, events driven communication, seamless integration to NI Labview, Matlab, Igor scientific toolboxes or OPC-UA plc, EPICS bus, ...