Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard TANGO Control System Gateway
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 362 subscribers
  • Views 748 views
  • Users 0 members are here
Related

Zedboard TANGO Control System Gateway

e14 Contributor
e14 Contributor over 11 years ago

accessing ZedBoard PL from TANGO distributed control system

youtube video https://youtu.be/fH60xha-u6o


paper here : https://docs.google.com/document/d/1HOfuCSrw6B209dEPM7wvXpxm8jWtyQ9mt2t3AShQnJI


Download a ready to launch TangoBox (64 bit OS / VirtualBox required, 1.4GB)
http://dl.free.fr/dWfRMq6Xe
flash zedboard qspi memory with BOOT.bin
http://dl.free.fr/b5O2C4K43

see www.tango-controls.org for more info on TANGO Control system and www.esrf.eu where it was designed and used since 1996.

Tango is a free, open source, distributed, scalable, efficient SCADA framework : a set of tools and API to monitor industrial appliance of any kinds...
Tango control system was elaborated at the ESRF, a large synchrotron radiation facility in Grenoble, France. The ESRF is a large research laboratory (1500 engineers, researchers, ), a kind of giant microscope to explore organic molecules or others and that uses X rays of high energy (6 GeV) issued from an 850 meters circumference accelerator in more than 40 beams lines operating simultaneously. see www.esrf.eu for info.

Tango Control System is a 100 man/years middleware, which aims at the monitoring 24/7 of more than 200 000 sensors & actuators in the facility. It features among other usage : logging, events driven communication, seamless integration to NI Labview, Matlab, Igor scientific toolboxes or OPC-UA plc, EPICS bus, ...

The SKA Telescope (square kilometre array telescope in southAfrica/Australia) will use TANGO. (skatelescope.org)
But Tango can also fit in a raspberry pi or in a zynq SoC ! But it is a serious game...

we enroll in XUP OpenHardware 2015 Contest with this proof of concept.
thank you for reading

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago
        Dear all,
       
        we registered again a team from the class "Lpro Systèmes embarqués" UJF Grenoble in the Xilinx University Contest, OpenHardware 2016 (http://www.openhw.eu/)
       
        our project is the AmpereHourMeter Tango device server (aka Bouteillometer) revamping… This device is measuring current in TFL (Radiation Dose estimation in Transfer line 1 & 2) of the ESRF.
       
        this proof of concept is built with a ZedBoard (Xilinx SoC Zynq 7020), featuring :
       
       
          
    •       Assymetric MultiProcessor : one ARM core for linux/tango device server and use the other one for a standalone bare metal app driving interlock (human safety can't rely on a non deterministic linux app)
    •     
    •       use Zynq internal XADC
    •     
    •       Communication between cores use Xilinx On Chip Memory
    •     
    •       Linux is custom Openembedded.
    •    
       
       
        Youtube here... with demo files
        paper here :
        https://docs.google.com/document/d/1glvFaKJogfreaWkISOiwTDw1JLJJtfZDZQDQ5kmIFsI
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago
        Dear all,
       
        we registered again a team from the class "Lpro Systèmes embarqués" UJF Grenoble in the Xilinx University Contest, OpenHardware 2016 (http://www.openhw.eu/)
       
        our project is the AmpereHourMeter Tango device server (aka Bouteillometer) revamping… This device is measuring current in TFL (Radiation Dose estimation in Transfer line 1 & 2) of the ESRF.
       
        this proof of concept is built with a ZedBoard (Xilinx SoC Zynq 7020), featuring :
       
       
          
    •       Assymetric MultiProcessor : one ARM core for linux/tango device server and use the other one for a standalone bare metal app driving interlock (human safety can't rely on a non deterministic linux app)
    •     
    •       use Zynq internal XADC
    •     
    •       Communication between cores use Xilinx On Chip Memory
    •     
    •       Linux is custom Openembedded.
    •    
       
       
        Youtube here... with demo files
        paper here :
        https://docs.google.com/document/d/1glvFaKJogfreaWkISOiwTDw1JLJJtfZDZQDQ5kmIFsI