Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design DMASlvErr in AXI CDMA
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 667 views
  • Users 0 members are here
Related

DMASlvErr in AXI CDMA

e14 Contributor
e14 Contributor over 13 years ago

Hello everybody!

I'm trying to work with AXI CDMA but I'm facing an error that I'm not able to solve. I read chapter 6 in "Zynq-7000 All Programmable SoC: Concepts, Tools and Techniques (CTT)" and instatiated a CDMA in the PL. I used HP1 and HP3 instead of HP0 and HP2. I configured base and high address for HP1 as 0x00000000 and 0x00000FFF, while base and high address for HP3 are 0x00003000 and 0x00003FFF. Then I wrote a simple C program that initializes source and destination memories, programs DMA and reads destination memory after a transfer has been finished.

Results: destination memory contains original values, like no trasfer has been executed, and the status register contains (bit 14 to 0) 101000000100010, wich means: interrupts are generated (bit 14 and 12), DMASlvErr (bit 5) and idle status (bit 1).

I don't understand why the CDMA raises that error. Maybe I miss something?

Thanks in advance,

sticken

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hello Sticken,
    I am beginner to ZYNQ APP platform and i am trying to configure DMA controller to start the transaction between any IP on PL with memories on PS. can you share with me the C code with which you programmed and configured DMA. I need just a starting point as i am stuck. I am now familiar with XPS and SDK which i had never used before. Any help will be welcomed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    The addresses of your HP ports may be outside the DDR address range.  In my address map ps7_ddr_0 goes from 0x00100000 to 0x1fffffff.  Your addresses should fall in that range.