Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design accessing Usb Uart pins through PL
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 361 subscribers
  • Views 580 views
  • Users 0 members are here
Related

accessing Usb Uart pins through PL

thala7
thala7 over 9 years ago

Hi,

I am working with leon3 Zedboard template Design on Zedboard for my project.

I want  to use Usb Uart pins for  uart communication between my hardware logic and my pc.

I have tried with different  possible locations of Uart D11,C14,D12,B10. and also I have tried Pmod pin locations to use it as pmod Uart converter.

I have ended up with this error :

ERROR: [Drc 23-20] Rule violation (UCIO-1) Unconstrained Logical Port - 2 out of 152 logical ports have no user assigned specific location constraint (LOC). This may cause I/O contention or incompatibility with the board power or connectivity affecting performance, signal integrity or in extreme cases cause damage to the device or the components to which it is connected. To correct this violation, specify all pin locations. This design will fail to generate a bitstream unless all logical ports have a user specified site LOC constraint defined.  To allow bitstream creation with unspecified pin locations (not recommended), use this command: set_property SEVERITY {Warning} [get_drc_checks UCIO-1].  NOTE: When using the Vivado Runs infrastructure (e.g. launch_runs Tcl command), add this command to a .tcl file and add that file as a pre-hook for write_bitstream step for the implementation run.  Problem ports: uart_tx, uart_rx.

Could you Please provide me a solution to get the uart  output to pc from PL.

Thank you

With best regards

Thala7

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Thala7,

    I am going to request that you ask this question over at the digilent forum as they are the main point of contact for educational support.

    https://forum.digilentinc.com/

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • thala7
    0 thala7 over 9 years ago in reply to jafoste4

    ok,Thank you Josh for your response.

    with regards,

    Thala7