Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design spi device clock problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 359 subscribers
  • Views 1903 views
  • Users 0 members are here
Related

spi device clock problem

e14 Contributor
e14 Contributor over 10 years ago

Hello
I am working with 7z020 board and using vivado 2015.2 version as well as petalinux 2015.2
I want to send /receive data from spi device, (in half duplex mode)for this purpose,I made the following connections.

set_property PACKAGE_PIN R19 [get_ports SPI0_MOSI_O]
set_property PACKAGE_PIN D18 [get_ports SPI0_SCLK_O]
set_property PACKAGE_PIN L21 [get_ports SPI0_SS_O]

set_property PACKAGE_PIN E21 [get_ports SPI1_MISO_I]
set_property PACKAGE_PIN L18 [get_ports SPI1_SCLK_O]
set_property PACKAGE_PIN F18 [get_ports SPI1_SS_O]

SPI1_SS_O and SPI0_SS_O is always high as I was expecting (will be low during transfer)
but cannot see clock at L18(FMC H4 pin) and D18(FMC G2 pin)
then I tried predefined softwarelike spidev_test.c i made it simple  I was trying to run the
#include <stdio.h>
#include <stdlib.h>
#include <stdint.h>
#include <errno.h>
#include <unistd.h>
#include <fcntl.h>
#include <malloc.h>
#include <string.h>
#include <sys/types.h>
#include <sys/ioctl.h>
#include <signal.h>
#include <linux/spi/spidev.h>

#define ARRAY_SIZE(a) (sizeof(a) / sizeof((a)[0]))

static void pabort(const char *s)
{
  perror(s);
  abort();
}

static const char *device = "/dev/spidev2.0";
static uint8_t mode;
static uint8_t bits = 1;
static uint32_t speed = 18000000;
//static uint16_t delay;

static void transfer(int fd)
{
  int ret,i;
  uint8_t tx[] = {0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF,
          0x40, 0x00, 0x00, 0x00, 0x00, 0x95,
          0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF,
          0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF,
          0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF,
          0xDE, 0xAD, 0xBE, 0xEF, 0xBA, 0xAD,
          0xF0, 0x0D,
  };
  uint8_t rx[ARRAY_SIZE(tx)] = {0, };
  struct spi_ioc_transfer tr = {
    .tx_buf = (unsigned long)tx,
    .rx_buf = (unsigned long)rx,
    .len = ARRAY_SIZE(tx),
    .delay_usecs = 50,
    .speed_hz = speed,
    .bits_per_word = bits,
    .cs_change=1,
  };
  
      ret = ioctl(fd, SPI_IOC_MESSAGE(0), &tr);
              if (ret < 0)
              {
                printf("return=%d
",ret);
                pabort("can't send spi message");
              }
        printf("
receive data");
            for (ret = 0; ret < ARRAY_SIZE(tx); ret++)
            {
                if (!(ret % 6))
                puts("");
                printf("%.2X ", rx[ret]);
            }
     
}

int main(int argc, char *argv[])
{
  int ret = 0;
  //int i;
  int fd;

  fd = open(device, O_RDWR);
  if (fd < 0)
    pabort("can't open device");

  mode = SPI_MODE_1;
  bits = 1;
  speed = 180000000;

  /*
   * spi mode
   */
  ret = ioctl(fd, SPI_IOC_WR_MODE, &mode);
  if (ret == -1)
    pabort("can't set spi mode");

  ret = ioctl(fd, SPI_IOC_RD_MODE, &mode);
  if (ret == -1)
    pabort("can't get spi mode");

  /*
   * bits per word
   */
  ret = ioctl(fd, SPI_IOC_WR_BITS_PER_WORD, &bits);
  if (ret == -1)
    pabort("can't set bits per word");

  ret = ioctl(fd, SPI_IOC_RD_BITS_PER_WORD, &bits);
  if (ret == -1)
    pabort("can't get bits per word");

  /*
   * max speed hz
   */
  ret = ioctl(fd, SPI_IOC_WR_MAX_SPEED_HZ, &speed);
  if (ret == -1)
    pabort("can't set max speed hz");

  ret = ioctl(fd, SPI_IOC_RD_MAX_SPEED_HZ, &speed);
  if (ret == -1)
    pabort("can't get max speed hz");

  printf("spi mode: %d
", mode);
  printf("bits per word: %d
", bits);
  printf("max speed: %d Hz (%d KHz)
", speed, speed/1000);
  printf("Now transfer data
");
  transfer(fd);

  close(fd);

  return ret;
}
then i got he following results
spi mode: 1
bits per word: 1
max speed: 180000000 Hz (180000 KHz)
Now transfer data

trying to transfer data

receive data data
00 00 00 00 00 00
00 00 00 00 00 00
00 00 00 00 00 00
00 00 00 00 00 00
00 00 00 00 00 00
00 00 00 00 00 00
00 00
where i am doing mistake? why i cant get clock?
Anyone help me
thanks in advance

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi
    thanks for your response. It really helping me,
    As you suggest I tried to do the same but I got the error
    Process STDIO not connected to console.
    If you'd like to see UART output in this console, please modify STDIO settings in the Run/Debug configuration.
    with the help of forum disussion i solved it and got another error
    connect STDIO to console :Jtag uart

    error opening jtag uart @ localhost-1 I was trying to solve it , the programm run and i got the following result (Idont know how it run, because again i am facing the same problem, and according to forum discussion sdk->xilinxtools->configuration of jtag I cannot find this option in sdk2015.2. any other solution?)

    http://s19.postimg.org/8q4292p2r/spi_not_working.png
    clearly shows that spiPsSelfTestExample() FAILED

    I am using picocom.
    is it my fault? or the board has some?
    In my opinion I just download the .bit file so error may be in the .bit file.
    have a look on the following pictures which shows my project

    http://s19.postimg.org/hh6hplj03/ps7_as.png

    http://s19.postimg.org/l8g2bwwoj/1_myproject.png

    http://s19.postimg.org/n1nkdz78z/2_myproject.png

    http://s19.postimg.org/px0nkub8z/3_myproject.png

    If you need to know more about my project , ask me.
    thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi
    thanks for your response. It really helping me,
    As you suggest I tried to do the same but I got the error
    Process STDIO not connected to console.
    If you'd like to see UART output in this console, please modify STDIO settings in the Run/Debug configuration.
    with the help of forum disussion i solved it and got another error
    connect STDIO to console :Jtag uart

    error opening jtag uart @ localhost-1 I was trying to solve it , the programm run and i got the following result (Idont know how it run, because again i am facing the same problem, and according to forum discussion sdk->xilinxtools->configuration of jtag I cannot find this option in sdk2015.2. any other solution?)

    http://s19.postimg.org/8q4292p2r/spi_not_working.png
    clearly shows that spiPsSelfTestExample() FAILED

    I am using picocom.
    is it my fault? or the board has some?
    In my opinion I just download the .bit file so error may be in the .bit file.
    have a look on the following pictures which shows my project

    http://s19.postimg.org/hh6hplj03/ps7_as.png

    http://s19.postimg.org/l8g2bwwoj/1_myproject.png

    http://s19.postimg.org/n1nkdz78z/2_myproject.png

    http://s19.postimg.org/px0nkub8z/3_myproject.png

    If you need to know more about my project , ask me.
    thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data