Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design PS I2C
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 360 subscribers
  • Views 739 views
  • Users 0 members are here
Related

PS I2C

e14 Contributor
e14 Contributor over 13 years ago

Hi Guys,

I want to use the PS I2C_0 to communicate through the PMOD interface. I selected the PMOD JE1. Pins JE9 and JE10 are connected to MIO14 and MIO15, so I created a design where I2C_0 is mapped to MIO14/15. I exported the design to SDK, created a BSP, and I am able to run software and see UART output.

However, when I try to use the PS I2C driver (interrupt or polled), it will cancel (interrupt) or stall forever (polled).

External pull-up is provided on both lines. The MIO14/15 IO config registers read
MIO 14: 0x00000640
MIO 15: 0x00000640
which looks okay to me.

When searching for a solution I found a chinese guy complaining about the very same problem (no solution):

http://group.chinaaet.com/109/61386

Any ideas?

Thanks in advance!

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 13 years ago

    Hi Rasfunk,

    Have you tried connecting an oscilloscope to pins JE9 and JE10 to see if there is any activity on the I2C lines?

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to zedhed

    Hi Kevin,
    thanks for your reply. I believe there is a constant 3.3V level on both clock and data. I'll re-measure on monday.

    One more thing: I am able to toggle output pins using the PS IO without any problems.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to zedhed

    Hi Kevin,
    thanks for your reply. I believe there is a constant 3.3V level on both clock and data. I'll re-measure on monday.

    One more thing: I am able to toggle output pins using the PS IO without any problems.