Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design How to store photos on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 360 subscribers
  • Views 541 views
  • Users 0 members are here
Related

How to store photos on Zedboard

e14 Contributor
e14 Contributor over 10 years ago

Hello

i'm only a begginer and i'm trying to figure out how to store 4 photos on Zedboard and then display it on the monitor via VGA using Matlab 2015 and vivado. I'm in over my head and need some guidance on how to get out.

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 10 years ago

    Hi Padma,

    To my knowledge, no one has ever done this before.

    That being said, most of the pieces already exist for what you want to do but there would be a lot of work to put it all together.

    I would recommend starting with getting the VGA portion working first.  Here is a post where that topic came up:

    http://microzed.org/content/displaying-image-using-vga-zedboard

    If you can use HDMI, I think that simplifies the task a bit because there are more examples of how to use the HDMI than there are of how to use the VGA.

    For either approach, you will are going to need some way to store the photo RGB data into DDR memory since the programmable logic (PL) available on the ZedBoard Zynq 7Z020 device does not have enough BRAM to store an entire 1920x1080 24-bit color image in memory.  Usually this is done through the use of a Frame Buffer where the PL can pull photo data from and stream it out to the ADV7511 HDMI output device.

    If you decide to go the HDMI route, I recommend looking into the reference design from the folks at ADI:

    https://wiki.analog.com/resources/fpga/xilinx/kc705/adv7511

    There is a demo program which will display an image and play a sound.  That demo program could then be modified to display your 4 photos.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to zedhed

    Thank you Sir, that was really helpfull