Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Share Data between cpu0 and cpu1
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 358 subscribers
  • Views 221 views
  • Users 0 members are here
Related

Share Data between cpu0 and cpu1

Former Member
Former Member over 10 years ago

1. I have used the design of zedboard XAPP1079 in which two baremetal application are run on two different cpu of zedboard.

2. Using that design i want to write data using CPU0 on ON-CHIP-MEMORY and read the same data using cpu1 From ON-CHIP-MEMORY. The code for the same is provided below.

3. Writing the data is done perfectly but while reading some garbage values are read as shown below.

4. Can anyone help on these?



CPU0:

#include <stdio.h>
#include "xil_io.h"
#include "xil_mmu.h"
#include "xil_exception.h"
#include "xpseudo_asm.h"
#include "xscugic.h"
#include "sleep.h"


#define INTCtt    XScuGic
#define INTC_DEVICE_IDtXPAR_PS7_SCUGIC_0_DEVICE_ID
#define INTC_HANDLERtXScuGic_InterruptHandler

#define sev() __asm__("sev")
#define CPU1STARTADR 0xfffffff0
#define COMM_VAL  (*(volatile unsigned long *)(0xFFFF0000))

static int  SetupIntrSystem(INTC *IntcInstancePtr);

INTC   IntcInstancePtr;

int main()
{
tint Status;
txil_printf("cpu0
");
    //Disable cache on OCM
    Xil_SetTlbAttributes(0xFFFF0000,0x14de2);           // S=b1 TEX=b100 AP=b11, Domain=b1111, C=b0, B=b0


    COMM_VAL = 0;
/////////////////////////////////////
    u32ti,j=0;
    u32thigh_addr=0x0020ffff;
    u32 readvalue,value=0,valuer=0;
//        init_platform();

        print("Hello World
r");
        xil_printf("High address=%d
", high_addr);

        tttfor(i=0x0020ff00;i<high_addr;i++)
        ttt{
        tttif(value==65537)
        ttttvalue=0;
        ttttXil_Out16(XPAR_DDR_MEM_BASEADDR+(2*i),value);
        tttxil_printf("value at address is %d
",value);
        tttvalue++;

                      }
    /////////////////////////////////////
t// Initialize the SCU Interrupt Distributer (ICD)
tStatus = SetupIntrSystem(&IntcInstancePtr);
tif (Status != XST_SUCCESS) {
ttreturn XST_FAILURE;
t}


    print("CPU0: writing startaddress for cpu1
r");
    Xil_Out32(CPU1STARTADR, 0x00200000);
    dmb(); //waits until write has finished

    print("CPU0: sending the SEV to wake up CPU1
r");
    sev();

    while(1){
    tsleep(5);
ttprint("CPU0: Hello World CPU 0
r");
ttsleep(5);
ttCOMM_VAL = 1;
ttwhile(COMM_VAL == 1);


    }

    return 0;
}


static int SetupIntrSystem(INTC *IntcInstancePtr)
{
tint Status;


tXScuGic_Config *IntcConfig;

t/*
t * Initialize the interrupt controller driver so that it is ready to
t * use.
t */
tIntcConfig = XScuGic_LookupConfig(INTC_DEVICE_ID);
tif (NULL == IntcConfig) {
ttreturn XST_FAILURE;
t}

tStatus = XScuGic_CfgInitialize(IntcInstancePtr, IntcConfig,
tttttIntcConfig->CpuBaseAddress);
tif (Status != XST_SUCCESS) {
ttreturn XST_FAILURE;
t}

t/*
t * Initialize the  exception table
t */
tXil_ExceptionInit();

t/*
t * Register the interrupt controller handler with the exception table
t */
tXil_ExceptionRegisterHandler(XIL_EXCEPTION_ID_INT,
ttt (Xil_ExceptionHandler)INTC_HANDLER,
ttt IntcInstancePtr);

t/*
t * Enable non-critical exceptions
t */
tXil_ExceptionEnable();


treturn XST_SUCCESS;
}



CPU1:

#include "xparameters.h"
#include <stdio.h>
#include "xil_io.h"
#include "xil_mmu.h"
#include "xil_cache.h"
#include "xil_exception.h"
#include "xscugic.h"
#include "sleep.h"


#define INTCtt    XScuGic
#define INTC_HANDLERtXScuGic_InterruptHandler
#define INTC_DEVICE_IDtXPAR_PS7_SCUGIC_0_DEVICE_ID
#define PL_IRQ_ID       XPS_IRQ_INT_ID

#define IRQ_PCORE_GEN_BASE  XPAR_IRQ_GEN_0_BASEADDR


#define COMM_VAL    (*(volatile unsigned long *)(0xFFFF0000))

/**
* This typedef contains configuration information for the device driver.
*/
typedef struct {
tu16 DeviceId;tt/**< Unique ID of device */
tu32 BaseAddress;t/**< Base address of the device */
} Pl_Config;


/**
* The driver instance data. The user is required to allocate a
* variable of this type.
* A pointer to a variable of this type is then passed to the driver API
* functions.
*/
typedef struct {
tPl_Config Config;   /**< Hardware Configuration */
tu32 IsReady;tt/**< Device is initialized and ready */
tu32 IsStarted;tt/**< Device is running */
} XPlIrq;


void        Xil_L1DCacheFlush(void);
static int  SetupIntrSystem(INTC *IntcInstancePtr, XPlIrq *PeriphInstancePtr, u16 IntrId);
static void DisableIntrSystem(INTC *IntcInstancePtr, u16 IntrId);
static void PlIntrHandler(void *CallBackRef);

extern u32 MMUTable;

/**
* Assign the driver structures for the interrupt controller and
* PL Core interrupt source
*/
INTC   IntcInstancePtr;
XPlIrq PlIrqInstancePtr;

// Global for IRQ communication to main()
int irq_count;


int main()
{
tint Status;

xil_printf("cpu1
");
    //Disable cache on OCM
tXil_SetTlbAttributes(0xFFFF0000,0x14de2);           // S=b1 TEX=b100 AP=b11, Domain=b1111, C=b0, B=b0


    print("CPU1: init_platform
r");

    irq_count = 0;

    // Initialize driver instance for PL IRQ
    PlIrqInstancePtr.Config.DeviceId = PL_IRQ_ID;
//    PlIrqInstancePtr.Config.BaseAddress = IRQ_PCORE_GEN_BASE;
    PlIrqInstancePtr.IsReady = XIL_COMPONENT_IS_READY;
    PlIrqInstancePtr.IsStarted = 0;


t/*
t * Connect the PL IRQ to the interrupt subsystem so that interrupts
t * can occur
t */

t////////////////////////////////////////////
t    u32tj=0;
t    u32thigh_addr=0x0020ffff;
t    u32 readvalue,valuer=0;
t//        init_platform();
t//        Xil_SetTlbAttributes(0xFFFF0000,0x14de2);

t        for(j=0x0020ff00;j<high_addr;j++)
t            ttt{
t            tttif(valuer==65537)
t            ttttvaluer=0;
t            tttreadvalue=Xil_In16(XPAR_DDR_MEM_BASEADDR+(2*j));
t            tttxil_printf("value_receive %d
",readvalue);
t            tttvaluer++;

t    }
t/////////////////////////////////////////////////////////////////////
tStatus = SetupIntrSystem(&IntcInstancePtr,
ttttt&PlIrqInstancePtr,
tttttPL_IRQ_ID);
tif (Status != XST_SUCCESS) {
ttreturn XST_FAILURE;
t}

     while(1){
     twhile(COMM_VAL == 0){};
     tif(irq_count > 0) {
         tprint("CPU1: Hello World With Interrupt CPU 1
r");
         tirq_count = 0;
         tsleep(2);tt//Delay so output can be seen
     t} else {
     ttsleep(5);
     tprint("CPU1: Hello World CPU 1
r");
     tsleep(5);
     t}
     tCOMM_VAL = 0;

     }

t/*
t * Disable and disconnect the interrupt system
t */
tDisableIntrSystem(&IntcInstancePtr, PL_IRQ_ID);


    return 0;
}

static int SetupIntrSystem(INTC *IntcInstancePtr,
ttXPlIrq *PeriphInstancePtr,
ttttu16 IntrId)
{
tint Status;


tXScuGic_Config *IntcConfig;

t/*
t * Initialize the interrupt controller driver so that it is ready to
t * use.
t */
tIntcConfig = XScuGic_LookupConfig(INTC_DEVICE_ID);
tif (NULL == IntcConfig) {
ttreturn XST_FAILURE;
t}

tStatus = XScuGic_CfgInitialize(IntcInstancePtr, IntcConfig,
tttttIntcConfig->CpuBaseAddress);
tif (Status != XST_SUCCESS) {
ttreturn XST_FAILURE;
t}

t/*
t * Connect the interrupt handler that will be called when an
t * interrupt occurs for the device.
t */
tStatus = XScuGic_Connect(IntcInstancePtr, IntrId,
tttt (Xil_ExceptionHandler)PlIntrHandler,
tttt PeriphInstancePtr);
tif (Status != XST_SUCCESS) {
ttreturn Status;
t}

t/*
t * Enable the interrupt for the PL device.
t */
tXScuGic_Enable(IntcInstancePtr, IntrId);


t/*
t * Initialize the  exception table
t */
tXil_ExceptionInit();

t/*
t * Register the interrupt controller handler with the exception table
t */
tXil_ExceptionRegisterHandler(XIL_EXCEPTION_ID_INT,
ttt (Xil_ExceptionHandler)INTC_HANDLER,
ttt IntcInstancePtr);

t/*
t * Enable non-critical exceptions
t */
tXil_ExceptionEnable();


treturn XST_SUCCESS;
}


static void PlIntrHandler(void *CallBackRef)
{

tXPlIrq *InstancePtr = (XPlIrq *)CallBackRef;

t/*
t * Clear the interrupt source
t */
tXil_Out32(InstancePtr->Config.BaseAddress, 0);

tirq_count = 1;

}




static void DisableIntrSystem(INTC *IntcInstancePtr, u16 IntrId)
{

t/*
t * Disconnect and disable the interrupt
t */
t/* Disconnect the interrupt */
tXScuGic_Disable(IntcInstancePtr, IntrId);
tXScuGic_Disconnect(IntcInstancePtr, IntrId);
}


RESULT:
cpu0
Hello World
High address=2162687
value at address is 0
value at address is 1
value at address is 2
value at address is 3
value at address is 4
value at address is 5
value at address is 6
value at address is 7
value at address is 8
value at address is 9
value at address is 10
value at address is 11
value at address is 12
value at address is 13
value at address is 14
value at address is 15
value at address is 16
value at address is 17
value at address is 18
value at address is 19
value at address is 20
value at address is 21
value at address is 22
value at address is 23
value at address is 24
value at address is 25
value at address is 26
value at address is 27
value at address is 28
value at address is 29
value at address is 30
value at address is 31
value at address is 32
value at address is 33
value at address is 34
value at address is 35
value at address is 36
value at address is 37
value at address is 38
value at address is 39
value at address is 40
value at address is 41
value at address is 42
value at address is 43
value at address is 44
value at address is 45
value at address is 46
value at address is 47
value at address is 48
value at address is 49
value at address is 50
value at address is 51
value at address is 52
value at address is 53
value at address is 54
value at address is 55
value at address is 56
value at address is 57
value at address is 58
value at address is 59
value at address is 60
value at address is 61
value at address is 62
value at address is 63
value at address is 64
value at address is 65
value at address is 66
value at address is 67
value at address is 68
value at address is 69
value at address is 70
value at address is 71
value at address is 72
value at address is 73
value at address is 74
value at address is 75
value at address is 76
value at address is 77
value at address is 78
value at address is 79
value at address is 80
value at address is 81
value at address is 82
value at address is 83
value at address is 84
value at address is 85
value at address is 86
value at address is 87
value at address is 88
value at address is 89
value at address is 90
value at address is 91
value at address is 92
value at address is 93
value at address is 94
value at address is 95
value at address is 96
value at address is 97
value at address is 98
value at address is 99
value at address is 100
value at address is 101
value at address is 102
value at address is 103
value at address is 104
value at address is 105
value at address is 106
value at address is 107
value at address is 108
value at address is 109
value at address is 110
value at address is 111
value at address is 112
value at address is 113
value at address is 114
value at address is 115
value at address is 116
value at address is 117
value at address is 118
value at address is 119
value at address is 120
value at address is 121
value at address is 122
value at address is 123
value at address is 124
value at address is 125
value at address is 126
value at address is 127
value at address is 128
value at address is 129
value at address is 130
value at address is 131
value at address is 132
value at address is 133
value at address is 134
value at address is 135
value at address is 136
value at address is 137
value at address is 138
value at address is 139
value at address is 140
value at address is 141
value at address is 142
value at address is 143
value at address is 144
value at address is 145
value at address is 146
value at address is 147
value at address is 148
value at address is 149
value at address is 150
value at address is 151
value at address is 152
value at address is 153
value at address is 154
value at address is 155
value at address is 156
value at address is 157
value at address is 158
value at address is 159
value at address is 160
value at address is 161
value at address is 162
value at address is 163
value at address is 164
value at address is 165
value at address is 166
value at address is 167
value at address is 168
value at address is 169
value at address is 170
value at address is 171
value at address is 172
value at address is 173
value at address is 174
value at address is 175
value at address is 176
value at address is 177
value at address is 178
value at address is 179
value at address is 180
value at address is 181
value at address is 182
value at address is 183
value at address is 184
value at address is 185
value at address is 186
value at address is 187
value at address is 188
value at address is 189
value at address is 190
value at address is 191
value at address is 192
value at address is 193
value at address is 194
value at address is 195
value at address is 196
value at address is 197
value at address is 198
value at address is 199
value at address is 200
value at address is 201
value at address is 202
value at address is 203
value at address is 204
value at address is 205
value at address is 206
value at address is 207
value at address is 208
value at address is 209
value at address is 210
value at address is 211
value at address is 212
value at address is 213
value at address is 214
value at address is 215
value at address is 216
value at address is 217
value at address is 218
value at address is 219
value at address is 220
value at address is 221
value at address is 222
value at address is 223
value at address is 224
value at address is 225
value at address is 226
value at address is 227
value at address is 228
value at address is 229
value at address is 230
value at address is 231
value at address is 232
value at address is 233
value at address is 234
value at address is 235
value at address is 236
value at address is 237
value at address is 238
value at address is 239
value at address is 240
value at address is 241
value at address is 242
value at address is 243
value at address is 244
value at address is 245
value at address is 246
value at address is 247
value at address is 248
value at address is 249
value at address is 250
value at address is 251
value at address is 252
value at address is 253
value at address is 254
CPU0: writing startaddress for cpu1
CPU0: sending the SEV to wake up CPU1
CPU0: Hello World CPU 0
cpu1
CPU1: init_platform
value_receive 53411
value_receive 49925
value_receive 49004
value_receive 15660
value_receive 22835
value_receive 21533
value_receive 26193
value_receive 3056
value_receive 59534
value_receive 49172
value_receive 32334
value_receive 35116
value_receive 36934
value_receive 8492
value_receive 21777
value_receive 22726
value_receive 523
value_receive 39514
value_receive 63601
value_receive 60565
value_receive 54644
value_receive 21328
value_receive 46629
value_receive 40337
value_receive 41096
value_receive 60929
value_receive 17331
value_receive 20480
value_receive 21795
value_receive 5319
value_receive 40209
value_receive 20451
value_receive 55698
value_receive 51042
value_receive 54567
value_receive 10371
value_receive 21517
value_receive 2054
value_receive 54777
value_receive 9017
value_receive 48801
value_receive 39
value_receive 12810
value_receive 20188
value_receive 13828
value_receive 24414
value_receive 19920
value_receive 52849
value_receive 3790
value_receive 46608
value_receive 35234
value_receive 53304
value_receive 51044
value_receive 6150
value_receive 5652
value_receive 41985
value_receive 45066
value_receive 37130
value_receive 14025
value_receive 44902
value_receive 61729
value_receive 21009
value_receive 3973
value_receive 36300
value_receive 3501
value_receive 21164
value_receive 44026
value_receive 21066
value_receive 27719
value_receive 16720
value_receive 53497
value_receive 7424
value_receive 9903
value_receive 32915
value_receive 43392
value_receive 2682
value_receive 61324
value_receive 55578
value_receive 11869
value_receive 3121
value_receive 39453
value_receive 29263
value_receive 22887
value_receive 32899
value_receive 28885
value_receive 13981
value_receive 58140
value_receive 6403
value_receive 3537
value_receive 34978
value_receive 52737
value_receive 20493
value_receive 1901
value_receive 31849
value_receive 20661
value_receive 50796
value_receive 13959
value_receive 33300
value_receive 43880
value_receive 26852
value_receive 13601
value_receive 51172
value_receive 55559
value_receive 16647
value_receive 24729
value_receive 8194
value_receive 35234
value_receive 41762
value_receive 5150
value_receive 23808
value_receive 50371
value_receive 36964
value_receive 51974
value_receive 38530
value_receive 13345
value_receive 30787
value_receive 30041
value_receive 52757
value_receive 39399
value_receive 20587
value_receive 53648
value_receive 14854
value_receive 8259
value_receive 50121
value_receive 31889
value_receive 16155
value_receive 5908
value_receive 60725
value_receive 16498
value_receive 8485
value_receive 13484
value_receive 28216
value_receive 21700
value_receive 50765
value_receive 21085
value_receive 21
value_receive 60330
value_receive 144
value_receive 4100
value_receive 48051
value_receive 60578
value_receive 20518
value_receive 10565
value_receive 2892
value_receive 14723
value_receive 1805
value_receive 18375
value_receive 38054
value_receive 25434
value_receive 14729
value_receive 51538
value_receive 42059
value_receive 625
value_receive 35108
value_receive 44993
value_receive 16974
value_receive 21777
value_receive 37713
value_receive 50371
value_receive 58408
value_receive 47306
value_receive 60846
value_receive 36758
value_receive 47182
value_receive 22385
value_receive 8236
value_receive 38869
value_receive 16718
value_receive 12939
value_receive 20
value_receive 35754
value_receive 35750
value_receive 24659
value_receive 35591
value_receive 57117
value_receive 13834
value_receive 49284
value_receive 32775
value_receive 91
value_receive 13394
value_receive 56420
value_receive 28757
value_receive 36000
value_receive 52547
value_receive 33009
value_receive 59399
value_receive 37385
value_receive 3329
value_receive 21509
value_receive 23588
value_receive 50504
value_receive 12699
value_receive 54938
value_receive 35849
value_receive 48644
value_receive 41620
value_receive 22449
value_receive 26957
value_receive 17492
value_receive 54135
value_receive 48784
value_receive 56768
value_receive 1068
value_receive 36909
value_receive 30297
value_receive 24308
value_receive 8205
value_receive 29401
value_receive 59530
value_receive 34077
value_receive 35926
value_receive 59764
value_receive 20805
value_receive 20836
value_receive 1321
value_receive 37051
value_receive 65036
value_receive 19460
value_receive 32971
value_receive 21018
value_receive 28933
value_receive 868
value_receive 50199
value_receive 159
value_receive 17125
value_receive 55315
value_receive 38801
value_receive 27340
value_receive 23893
value_receive 1539
value_receive 16900
value_receive 24648
value_receive 32159
value_receive 54200
value_receive 44590
value_receive 7691
value_receive 8036
value_receive 23606
value_receive 16465
value_receive 20925
value_receive 42297
value_receive 1814
value_receive 19997
value_receive 41867
value_receive 1296
value_receive 11130
value_receive 35638
value_receive 58628
value_receive 30630
value_receive 35008
value_receive 49165
value_receive 46213
value_receive 3410
value_receive 41675
value_receive 21285
CPU1: Hello World CPU 1
CPU0: Hello World CPU 0
CPU1: Hello World CPU 1
CPU0: Hello World CPU 0
CPU1: Hello World CPU 1