Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Avnet Zynq-7000 All Programmable SoC / AD9361 Software-Defined Radio Evaluation Kit
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 360 subscribers
  • Views 3362 views
  • Users 0 members are here
Related

Avnet Zynq-7000 All Programmable SoC / AD9361 Software-Defined Radio Evaluation Kit

e14 Contributor
e14 Contributor over 10 years ago

Hi ,

Had a few queries regarding the Zynq-7000 AP SoC / AD9361 Software-Defined Radio Systems Development Kit. We are in the process of identifying a platform that helps us test the performance of the AD9361, which we use as our radio board.

The two Development kits that we are looking at are the AES-ZSDR2-ADI-G and the AES-ZSDR3-ADI-G which work on the AD-FMCOMMS2-EBZ and the AD-FMCOMMS3-EBZ respectively.

Couple of questions though :

We have the AD-FMCOMMS3-EBZ already with us , we would like to know if the AES-ZSDR2-ADI-G development kit would work on the  AD-FMCOMMS3-EBZ FMC module , which means can we use the AES-ZSDR2-ADI-G to work and be compatible on a  AD-FMCOMMS3-EBZ  FMC modul ?

If not , the AES-ZSDR3-ADI-G seems to be working on the AD-FMCOMMS3-EBZ  FMC module  already , so in that case , we would like to know if we can just use the Xilinx ZynqRegistered-7000 All-Programmable SoC evalution kit and not purchase the AD-FMCOMMS3-EBZ  FMC module as we already have it ?

Please let me know if any more information is required.

 

Thanks .

  • Sign in to reply
  • Cancel
Parents
  • mbrown
    0 mbrown over 10 years ago

    Hi Krutika,

    The AES-ZSDR2-ADI-G is a kit that includes a ZedBoard carrier and an FMCOMMS2 module. ZedBoard is also compatible with FMCOMMS3.

     

    The AD9361_CLKOUT signal is connected to the Z7035 on bank 35, pin K12 (see below). The schematic is available on the docs page -- http://picozed.org/support/documentation/10511

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mbrown
    0 mbrown over 10 years ago

    Hi Krutika,

    The AES-ZSDR2-ADI-G is a kit that includes a ZedBoard carrier and an FMCOMMS2 module. ZedBoard is also compatible with FMCOMMS3.

     

    The AD9361_CLKOUT signal is connected to the Z7035 on bank 35, pin K12 (see below). The schematic is available on the docs page -- http://picozed.org/support/documentation/10511

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to mbrown

    Hi ,

    Thank you for your prompt reply.

    I understand that the AD9361_CLKOUT signal is connected to the Z7035 on bank 35, pin K12.

    But what we need is,  we would like to know if the  board has a test port or something like that for us to connect any test equipment such as a spectrum analyzer to test the functions oft the AD9361.

     

    Thank you

     

    -Kruttika .