Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Avnet Zynq-7000 All Programmable SoC / AD9361 Software-Defined Radio Evaluation Kit
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 360 subscribers
  • Views 3376 views
  • Users 0 members are here
Related

Avnet Zynq-7000 All Programmable SoC / AD9361 Software-Defined Radio Evaluation Kit

e14 Contributor
e14 Contributor over 10 years ago

Hi ,

Had a few queries regarding the Zynq-7000 AP SoC / AD9361 Software-Defined Radio Systems Development Kit. We are in the process of identifying a platform that helps us test the performance of the AD9361, which we use as our radio board.

The two Development kits that we are looking at are the AES-ZSDR2-ADI-G and the AES-ZSDR3-ADI-G which work on the AD-FMCOMMS2-EBZ and the AD-FMCOMMS3-EBZ respectively.

Couple of questions though :

We have the AD-FMCOMMS3-EBZ already with us , we would like to know if the AES-ZSDR2-ADI-G development kit would work on the  AD-FMCOMMS3-EBZ FMC module , which means can we use the AES-ZSDR2-ADI-G to work and be compatible on a  AD-FMCOMMS3-EBZ  FMC modul ?

If not , the AES-ZSDR3-ADI-G seems to be working on the AD-FMCOMMS3-EBZ  FMC module  already , so in that case , we would like to know if we can just use the Xilinx ZynqRegistered-7000 All-Programmable SoC evalution kit and not purchase the AD-FMCOMMS3-EBZ  FMC module as we already have it ?

Please let me know if any more information is required.

 

Thanks .

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi Gary , 

    As you had suggested , we are looking at the PicoZed SDR , i had a small query regarding the AD9361/Zynq Z-7035 Interface , 

    According to the block diagram of the AD9361/Zynq Z-7035 Interface in the following link :

    http://zedboard.org/sites/default/files/documentations/PicoZed%20SDR%20Z7035-AD9361%20SOM%20User's%20Guide%20v1.5.pdf

    (Page 17 , figure 7), we get a CLK_OUT from the AD9361 , could you tell us which pin it goes to in the Zynq Z-7035 and where can we locate it ?Do uou have any PIN_OUT diagram of the Zynq Z-7035 that you can provide us .

    Appreciate your help.

     

    -Kruttika

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi Gary , 

    As you had suggested , we are looking at the PicoZed SDR , i had a small query regarding the AD9361/Zynq Z-7035 Interface , 

    According to the block diagram of the AD9361/Zynq Z-7035 Interface in the following link :

    http://zedboard.org/sites/default/files/documentations/PicoZed%20SDR%20Z7035-AD9361%20SOM%20User's%20Guide%20v1.5.pdf

    (Page 17 , figure 7), we get a CLK_OUT from the AD9361 , could you tell us which pin it goes to in the Zynq Z-7035 and where can we locate it ?Do uou have any PIN_OUT diagram of the Zynq Z-7035 that you can provide us .

    Appreciate your help.

     

    -Kruttika