Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Avnet Zynq-7000 All Programmable SoC / AD9361 Software-Defined Radio Evaluation Kit
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 360 subscribers
  • Views 3368 views
  • Users 0 members are here
Related

Avnet Zynq-7000 All Programmable SoC / AD9361 Software-Defined Radio Evaluation Kit

e14 Contributor
e14 Contributor over 10 years ago

Hi ,

Had a few queries regarding the Zynq-7000 AP SoC / AD9361 Software-Defined Radio Systems Development Kit. We are in the process of identifying a platform that helps us test the performance of the AD9361, which we use as our radio board.

The two Development kits that we are looking at are the AES-ZSDR2-ADI-G and the AES-ZSDR3-ADI-G which work on the AD-FMCOMMS2-EBZ and the AD-FMCOMMS3-EBZ respectively.

Couple of questions though :

We have the AD-FMCOMMS3-EBZ already with us , we would like to know if the AES-ZSDR2-ADI-G development kit would work on the  AD-FMCOMMS3-EBZ FMC module , which means can we use the AES-ZSDR2-ADI-G to work and be compatible on a  AD-FMCOMMS3-EBZ  FMC modul ?

If not , the AES-ZSDR3-ADI-G seems to be working on the AD-FMCOMMS3-EBZ  FMC module  already , so in that case , we would like to know if we can just use the Xilinx ZynqRegistered-7000 All-Programmable SoC evalution kit and not purchase the AD-FMCOMMS3-EBZ  FMC module as we already have it ?

Please let me know if any more information is required.

 

Thanks .

  • Sign in to reply
  • Cancel
Parents
  • mbrown
    0 mbrown over 10 years ago

    AD9361_CLKOUT is only routed to the Zynq device. However, you could create a design using Xilinx Vivado software that routes the signal to a user I/O of the SOM and pick it up on a carrier card like the FMC Carrier or Breakout Carrier.

    The SOM also includes U.FL miniature coax connectors for all RF signals. That's where you could probe with your spectrum analyzer. The Development Kit ships with 2 U.FL-to-SMA cables that would make your connection easier.

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to mbrown

    Hi Matt , 

    Also the OTG cable provided in the kit , we connected it to the USB OTG port on the Zedboard , but it failed to recognize the mouse/keyboard.

    So we cannot access the IIO Oscilloscope after the boot up .

     

    Also we got a blank screeen with the " DIGILENT" logo after boot up .

    Could you kindly assist us with this .

     

    Thnaks ,

    Kruttika

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to mbrown

    Hi Matt , 

    Also the OTG cable provided in the kit , we connected it to the USB OTG port on the Zedboard , but it failed to recognize the mouse/keyboard.

    So we cannot access the IIO Oscilloscope after the boot up .

     

    Also we got a blank screeen with the " DIGILENT" logo after boot up .

    Could you kindly assist us with this .

     

    Thnaks ,

    Kruttika