Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Sampling external analog inputs with XADC
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 359 subscribers
  • Views 1295 views
  • Users 0 members are here
Related

Sampling external analog inputs with XADC

Former Member
Former Member over 13 years ago

I want to use XADC to sample 3 external analog inputs but the problem is that it can only sample internal signals like temperature or VCCs. When an external signal (of about 800 mV) is fed to VN/VP pins or auxiliary channel 0 or 8 at the XADC header, no data is captured by XADC. By the way, what is the correct way to connect an analog input to VN/VP or to any of the auxiliary channels.

FYI, I use AXI XADC 1.00a IP following the PlanAhead flow and XADC API driver in SDK to access XADC in simultaneous sampling mode (I have to remove MUXADDR, CONVST, and ALARM signals of the IP because PlanAhead won't generate bit stream with these signals hanging around).

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    Mr. Kang's lab exercises are very helpful. If you have trouble making any of them work, make sure you are using the same tool versions he did.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago

    Mr. Kang's lab exercises are very helpful. If you have trouble making any of them work, make sure you are using the same tool versions he did.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data