Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard Power with Current Sense
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 360 subscribers
  • Views 770 views
  • Users 0 members are here
Related

Zedboard Power with Current Sense

eactor
eactor over 12 years ago

Hello,
did anybody try to estimate the power consumption of the Zedboard using the onboad current sense J21?
If I but my Osciloscope on the those pins I'm measuring 3.2mV?
But how does that relate to the power drawn?
P=U^2/R  -> With the resitance beeing 10mOhm?
Using this would result in a power consumption below mW which seems unrealistic.
Cheers
eactor

I also checkt if the board is sneaking power elsewhere USB, PowerOverEthernet ... but without luck

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 12 years ago

    ZedBoard doesn't have multiple power sources, so the measurement across J21 should be accurate. The resistance in R292 is 10m-OHM, although the correct part number to use is Stackpole CSR1206FK10L0. This is a 1%, 0.5W, 1206 SMD resistor.

     

    http://www.seielect.com/Catalog/SEI-CSR_CSRN.pdf

     

    Based on your measurement of 3.2 mV across a 10m-ohm resistor, you can measure the current as I = V/R = 320mA. Since the input voltage source is 12V, you can calculate the power input to the board as P = I*V (V=12V, not the V you measured). So...

     

    P = 320mA * 12V = 3.84 W

     

    Are you running the default, out-of-box design that ships with ZedBoard?

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 12 years ago

    ZedBoard doesn't have multiple power sources, so the measurement across J21 should be accurate. The resistance in R292 is 10m-OHM, although the correct part number to use is Stackpole CSR1206FK10L0. This is a 1%, 0.5W, 1206 SMD resistor.

     

    http://www.seielect.com/Catalog/SEI-CSR_CSRN.pdf

     

    Based on your measurement of 3.2 mV across a 10m-ohm resistor, you can measure the current as I = V/R = 320mA. Since the input voltage source is 12V, you can calculate the power input to the board as P = I*V (V=12V, not the V you measured). So...

     

    P = 320mA * 12V = 3.84 W

     

    Are you running the default, out-of-box design that ships with ZedBoard?

     

    Bryan