Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design XPS VS VIVADO IPI (Microblaze & Zynq)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 671 views
  • Users 0 members are here
Related

XPS VS VIVADO IPI (Microblaze & Zynq)

e14 Contributor
e14 Contributor over 12 years ago

In Ug898 Vivado embedded design page-8 state that "The Vivado IP integrator is the replacem ent for Xilinx Platform Studio (XPS) for embedded processor designs, including designs targeting Zynq devices and MicroBlazeu2122 processors.XPS only supports designs targeting MicroBlaze processors".
While this states that XPS only supports Microblaze processors but on the other hand the application note #1093 demonstartes Microblaze & zynq processors in one design using XPS which mean XPS do support Zynq!! Am i right?
I will be thankful for sharp response-

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The XAPP1093 app note targets the ISE/PlanAhead 14.5 Xilinx tool suite, which does use XPS to support both Zynq and MicroBlaze designs. 

    The IP Integrator flow described in UG898 is in the Xilinx Vivado tool suite, which does use the Vivado IP Integrator to implement Zynq designs.

     

    In any case UG898 is a Xilinx document and xapp1093 is a Xilinx app note targeting the Xilinx ZC702 evaluation board, not a ZedBoard, so your question  would be better directed to the Xilinx community forums.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The XAPP1093 app note targets the ISE/PlanAhead 14.5 Xilinx tool suite, which does use XPS to support both Zynq and MicroBlaze designs. 

    The IP Integrator flow described in UG898 is in the Xilinx Vivado tool suite, which does use the Vivado IP Integrator to implement Zynq designs.

     

    In any case UG898 is a Xilinx document and xapp1093 is a Xilinx app note targeting the Xilinx ZC702 evaluation board, not a ZedBoard, so your question  would be better directed to the Xilinx community forums.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks-The Zedboard and XC702 has same structure as both are Zynq-7000 devices-Majority of applications running on XC702 should run on Zedboard if fits to its resources