Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design 1V power rail burnt ...
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 361 subscribers
  • Views 709 views
  • Users 0 members are here
Related

1V power rail burnt ...

e14 Contributor
e14 Contributor over 13 years ago

Hi,


Within a few minutes of operation, the zedboard ceased to operate all together, no leds even come up anymore.

A bit of diagnostic shows that the 1V rails is no longer operating. Here's what it looks like : http://i.imgur.com/klrQhI6.png  (so roughly 400 mv, and not stable). It's not really consuming any current (barely 10 ma).

Did anyone ever see such a failure ?  And what could cause it ?  I don't see any physical damage on the board, nor any obvious burnt component.

Cheers,

    Sylvain

  • Sign in to reply
  • Cancel
Parents
  • ctammann
    0 ctammann over 13 years ago

    We've recently gotten some reports from the field that some customers have seen their 1V supplies drawing upwards of 3A.  In all of our worst case calculations the highest current we expected to see based on the XPE tool was 1.3A.  We're investigating now on where this additional current draw is coming from.  Looking back at the issue you had with your system I wonder if perhaps you were also drawing higher current which could have caused the output inductor to saturate and damage something on the 1V rail.  Were you running your own build inside the device or did it fail without the Zynq device being loaded?
    Thanks
    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ctammann
    0 ctammann over 13 years ago

    We've recently gotten some reports from the field that some customers have seen their 1V supplies drawing upwards of 3A.  In all of our worst case calculations the highest current we expected to see based on the XPE tool was 1.3A.  We're investigating now on where this additional current draw is coming from.  Looking back at the issue you had with your system I wonder if perhaps you were also drawing higher current which could have caused the output inductor to saturate and damage something on the 1V rail.  Were you running your own build inside the device or did it fail without the Zynq device being loaded?
    Thanks
    Chris