Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design When to setup AXI DMA
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 358 subscribers
  • Views 215 views
  • Users 0 members are here
Related

When to setup AXI DMA

e14 Contributor
e14 Contributor over 11 years ago

I have a custom HW setup built around an AXI DMA block to implement a streaming interface, on which I'm intending to boot Linux. 

What I've noticed is that if I don't configure the AXI DMA HW before booting the kernel, the boot process hangs when loading the linux AxiDma driver, as it tries to write to the registers of an unconfigured device.

I can configure the AxiDma IP block in the FSBL (as long as  ps7_post_config() has run -- either from TCL or C).  I guess I could also move this init code into u-boot, or maybe even the linux kernel.

What's the recommend place for such code in the standard Xilinx/Zedboard software flow.