Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Serial cable is known under ttyACM0/1
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 354 subscribers
  • Views 634 views
  • Users 0 members are here
Related

Serial cable is known under ttyACM0/1

Former Member
Former Member over 13 years ago

Hi

When I connect ZED Board to the computer,
its serial link will be recognized as
/dev/ttyACM0 or /dev/ttyACM1 device.

However for ZC702, it is knows as /dev/ttyUSB0

I want to know the source of this difference?

Why for the ZED Board we don't simply have /dev/ttyUSB0 again?

Because /dev/ttyACM0 has a lot of problems. For example, when I turn of the board I should exit Minicom.
And then next time that I turn on the board it appears as ttyACM1 not 0 and i should reconfigure every thing again

do you know any solution to this?
thanks

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 13 years ago

    mamsadegh,

    My appologies it took so long to get back to you - as I wanted to confirm with the factory the modes of operation you were seeing.

    The thing that the factory found, and I confirmed, is that minicom is holding onto the handle and keeping the /dev/ttyACM0 'file' open.  Thus, when the kernel tries to enumerate the Cypress USB-UART bridge after a power cycle, it can not open the /dev/ttyACM0 file and errors out.  It would appear that the driver then falls over to see if it can open the next available 'file', called /dev/ttyACM1 - which works.

    The solution is to write out your minicom configuration to a script, and launch it that way.  Then close out, power cycle the board, and finally relaunch minicom.

    Let me know if you are successful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 13 years ago

    mamsadegh,

    My appologies it took so long to get back to you - as I wanted to confirm with the factory the modes of operation you were seeing.

    The thing that the factory found, and I confirmed, is that minicom is holding onto the handle and keeping the /dev/ttyACM0 'file' open.  Thus, when the kernel tries to enumerate the Cypress USB-UART bridge after a power cycle, it can not open the /dev/ttyACM0 file and errors out.  It would appear that the driver then falls over to see if it can open the next available 'file', called /dev/ttyACM1 - which works.

    The solution is to write out your minicom configuration to a script, and launch it that way.  Then close out, power cycle the board, and finally relaunch minicom.

    Let me know if you are successful.