Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design SDRAM Missing Pin
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 523 views
  • Users 0 members are here
Related

SDRAM Missing Pin

Former Member
Former Member over 13 years ago

In reviewing the Sept. 13 schematic I noticed that it appears as if pins F1 (VDDQ) and G7 (VDD) on the SDRAM are missing.  Also, I notice that T7 (NC) is listed as A14.  I understand that T7 may be used as A14 for another SDRAM chip, but why do F1 and G7 not appear on the schematic?

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 13 years ago

    Thank you very much for your feedback.  On Rev C ZedBoard, pins F1 and G7 on the two DDR3 chips are No-Connects.  This is why they do not show on the schematic.  This is an error.  F1 should be VDDQ, and G7 should be VDD, both of which should attach to the DDR1V5 rail.

     

    I have asked Micron for a statement of impact and received the following reply:

    It will be somewhat dependent on the board layout. If the supply distribution is robust enough to the other pins, and the signal integrity is adequate, there may not be a problem.  Once the board is running I would not expect to see problems develop in the field.  As for long term reliability, I don’t think the lack of a power connection to those pins will lead to long-term failures (on-die metal migration, etc.), especially operating at 533MHz.

     

    We will correct this during our next board revision.  Any designer that is using ZedBoard as a reference should connect these pins.  However, we do not expect it to be a problem on the existing Rev C boards in the field.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 13 years ago

    Thank you very much for your feedback.  On Rev C ZedBoard, pins F1 and G7 on the two DDR3 chips are No-Connects.  This is why they do not show on the schematic.  This is an error.  F1 should be VDDQ, and G7 should be VDD, both of which should attach to the DDR1V5 rail.

     

    I have asked Micron for a statement of impact and received the following reply:

    It will be somewhat dependent on the board layout. If the supply distribution is robust enough to the other pins, and the signal integrity is adequate, there may not be a problem.  Once the board is running I would not expect to see problems develop in the field.  As for long term reliability, I don’t think the lack of a power connection to those pins will lead to long-term failures (on-die metal migration, etc.), especially operating at 533MHz.

     

    We will correct this during our next board revision.  Any designer that is using ZedBoard as a reference should connect these pins.  However, we do not expect it to be a problem on the existing Rev C boards in the field.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data