Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design RevD booting
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 407 views
  • Users 0 members are here
Related

RevD booting

Former Member
Former Member over 12 years ago

  A simple hello world project which boots from SD on the RevC board, will not boot on the RevD board. The DDR3 is different on the RevD. Therefore, I revised the board definition file to account for the DDR3 and created a custom hardware platform in EDK for the RevD, export it to the SDK hello world project, compiled, created new boot.bin and try it on the RevD, but it still does not work. The linux image on the SD that came with board works and boots fine, but I can't get a bare metal application to work. Can anyone explain why this is happening? Is there something else that is missing in the RevD board definition file that must be revised?

I was able to run the hello world application through PROG usb (J17).

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 12 years ago

    The DDR3 on the Rev D is backwards compatible with the DDR3 on Rev C, so those changes weren't necessary. The biggest change going to Rev D was the switch to production silicon.

    •   Zynq C and CES are essentially compatible in every way except  
          
      •     JTAG ID http://www.xilinx.com/support/answers/37579.htm
      •   
      •     Timing (production timing first appeared in 14.4 w/ Device Pack http://www.xilinx.com/support/answers/54044.htm)
      •   
      •     Correction of errata http://www.xilinx.com/support/answers/47916.htm
      •  
    •   Designs that were working for CES will likely work with C devices with no change as long as the application isn’t explicitly checking for the CES JTAG ID
    •   If migrating older designs to the newer tools to achieve production timing, beware of tool migration issues:  
          
      •     http://www.xilinx.com/support/answers/51807.htm
      •  
    •   New designs created in 14.5 for C-grade ZedBoard are fully backward compatible with the CES boards (as long as you aren’t exercising the JTAG ID or something in the errata)

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 12 years ago

    The DDR3 on the Rev D is backwards compatible with the DDR3 on Rev C, so those changes weren't necessary. The biggest change going to Rev D was the switch to production silicon.

    •   Zynq C and CES are essentially compatible in every way except  
          
      •     JTAG ID http://www.xilinx.com/support/answers/37579.htm
      •   
      •     Timing (production timing first appeared in 14.4 w/ Device Pack http://www.xilinx.com/support/answers/54044.htm)
      •   
      •     Correction of errata http://www.xilinx.com/support/answers/47916.htm
      •  
    •   Designs that were working for CES will likely work with C devices with no change as long as the application isn’t explicitly checking for the CES JTAG ID
    •   If migrating older designs to the newer tools to achieve production timing, beware of tool migration issues:  
          
      •     http://www.xilinx.com/support/answers/51807.htm
      •  
    •   New designs created in 14.5 for C-grade ZedBoard are fully backward compatible with the CES boards (as long as you aren’t exercising the JTAG ID or something in the errata)

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 12 years ago in reply to bhfletcher

    Thanks!
    I managed to boot an RSA authenticated image from SD, but now I can not get the same image to boot from QSPI. When I use the XMD to read out the reboot_status[15:0], I get a BootROM error code of 0xE00C. I cannot decipher this code because its not listed under the BootROM error code table 6-12 in the TRM. Any clues what this error code is?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer