Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design 1V power supply issues
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 358 subscribers
  • Views 146 views
  • Users 0 members are here
Related

1V power supply issues

e14 Contributor
e14 Contributor over 13 years ago

I have used the Zedboard a bit and I have found that 1V PSU is under-powered when running large FPGA design. 1.2A is budgeted for the PL of the Zynq, but I have made some design that require more than that.
http://www.louif.com/power_analysis.png
When this design is loaded to the Zedboard, it causes a reset because the power supply failed. See voltage measured at C357.
http://www.louif.com/ADS00001.BMP
Also, I have disconnected MAX15021ATI+ chip and connected an external power supply. This solved the reset issue. I saw from the reading that as much as 3A can be drawn from the 1V PSU, but the MAX15021ATI+ can only provide 2A.
Is there any plan for a new revision of this board? I would very much like to see an improved 1V power supply. It would improve the Zedboard functionality.