Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard Digital to analog converter (DAC)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 1678 views
  • Users 0 members are here
Related

Zedboard Digital to analog converter (DAC)

e14 Contributor
e14 Contributor over 9 years ago

Hi

I want to purchase the zedboard for my application.

I Have to interface a conditioning  circuit at DAC output.

Kindly let me know what is the output voltage of DAC. 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Hello SDR1,

    The ZedBoard does not have a DAC circuit on the main board. You can add a DAC interface by using one of the PMOD expansion headers or the FMC expansion connector. The FMC connector is a Low Pin Count (LPC) interface, so make sure you select an expansion board that works with the LPC pinout if you use the FMC interface.

    The the interface between the ZedBoard and the PMOD interface is set to 3.3V. The FMC interface can be set to 3.3V, 2.5V, or 1.8V, based on the position of the VADJ jumpers on the ZedBoard. The interface between the DAC and your signal interface will depend on the interface PMOD or FMC board you choose.

    Maxim has several PMODs with DAC outputs:

    https://www.maximintegrated.com/en/design/design-technology/fpga-design-resources/pmod-compatible-plug-in-peripheral-modules.html

    http://zedboard.org/accessories/pmod

    Analog Devices has both PMOD and FMC boards with DAC outputs:

    http://www.analog.com/en/design-center/reference-designs/hardware-reference-design/fpga-compatible-reference-designs.html#xilinx

    And there is a list of FMC boards on the Xilinx website. Be careful to select one that supports the ZedBoards LPC FMC interface:

    http://www.xilinx.com/products/boards-and-kits/fmc-cards.html

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Hello SDR1,

    The ZedBoard does not have a DAC circuit on the main board. You can add a DAC interface by using one of the PMOD expansion headers or the FMC expansion connector. The FMC connector is a Low Pin Count (LPC) interface, so make sure you select an expansion board that works with the LPC pinout if you use the FMC interface.

    The the interface between the ZedBoard and the PMOD interface is set to 3.3V. The FMC interface can be set to 3.3V, 2.5V, or 1.8V, based on the position of the VADJ jumpers on the ZedBoard. The interface between the DAC and your signal interface will depend on the interface PMOD or FMC board you choose.

    Maxim has several PMODs with DAC outputs:

    https://www.maximintegrated.com/en/design/design-technology/fpga-design-resources/pmod-compatible-plug-in-peripheral-modules.html

    http://zedboard.org/accessories/pmod

    Analog Devices has both PMOD and FMC boards with DAC outputs:

    http://www.analog.com/en/design-center/reference-designs/hardware-reference-design/fpga-compatible-reference-designs.html#xilinx

    And there is a list of FMC boards on the Xilinx website. Be careful to select one that supports the ZedBoards LPC FMC interface:

    http://www.xilinx.com/products/boards-and-kits/fmc-cards.html

    -Gary