Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design PC communication - Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 360 subscribers
  • Views 494 views
  • Users 0 members are here
Related

PC communication - Zedboard

verbiesj
verbiesj over 10 years ago

Hello,

Applications:
1. a program written in C++ on a windows PC send out commands to the Zedboard. Depending on the command a number, letter or number letter combination will be displayed on an PmodSSD, a seven-segment display.

Today, it is not clear how to start. Tips, starting points are welcome.

2. I use the switches on the Zedboard to display a letter or number combination on the display and use the same C++ program to read out which letter or number is written on the display.

Today, it is not clear how to start. Tips, starting points are welcome.

Note: The idea is to do this using the USB.

Thanks.

Regards,
JrV

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 10 years ago

    When you say USB, do you mean USB 2.0 or USB-UART?

     

    USB-UART would be a lot easier. If you choose to go the USB 2.0 route, you need to learn how to set up the ZedBoard as a USB Device, and you will likely need to use Linux.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • verbiesj
    0 verbiesj over 10 years ago in reply to bhfletcher

    The idea is USB-UART.

    The idea is to send the needed commands/instructions to the Zedboard so the PL (FPGA) of PS+PL (ARM + FPGA) can perform the needed actions.



    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago

    Hi J,

      There are numerous examples for reading/writing from a serial port on Zynq (USB-UART).  Once you can read incoming data from your PC over the serial connection, you can then perform whatever local actions you wish in your standalone program.   Here is a post that will get you started with serial communication:

    https://forums.xilinx.com/t5/Embedded-Development-Tools/how-to-read-data-and-print-it-from-the-serial-port-using/td-p/186446

    The Xilinx drivers included with the SDK come complete with example code for invoking all the different APIs.  Just take a look at the installation hierarchy for the source code.  For example, in the 2015.2 installation, see:

    <Xilinx Tool Install Dir>\SDK\2015.2\data\embeddedsw\XilinxProcessorIPLib\drivers\uartps_v2_2\examples

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer