Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Reading the value of switches
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 1244 views
  • Users 0 members are here
Related

Reading the value of switches

e14 Contributor
e14 Contributor over 11 years ago

Hello, I have got vivado 2014.2 and zedboard..


I want to control the leds by the switches,  but also to use the switches for other purpose in vhdl , how i do this? And also, where can I find the location of the switches /less?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    It is not clear exactly what you are trying to implement but I will suggest a couple of options.

     

    You could set up both an 8 bit GPIO input port, connected to the ZedBoard switches, and an 8 bit GPIO output port, connected to the ZedBoard LEDs, and then write 'C' code to read from the 'switches' GPIO port and then write to the 'LEDs' GPIO port. You could do this using either the Zynq PS (Processing System) GPIO or by instantiating AXI GPIO IP blocks in the PL (Programable Logic). In either case the easiest thing to do is let the Vivado tools set the port addresses and use the logical addresses defined. There are a couple of good examples on how to do this using the PS GPIO in two of Adam Taylor's blog entries:

     

    http://forums.xilinx.com/t5/Xcell-Daily-Blog/Using-the-MicroZed-Button-for-Input-Adam-Taylor-s-MicroZed/ba-p/393035

    http://forums.xilinx.com/t5/Xcell-Daily-Blog/Driving-the-Zynq-SoC-s-GPIO-Adam-Taylor-s-MicroZed-Chronicles/ba-p/389611

     

    The other approach would be to design an HDL (VHDL or Verilog) block of logic that would take the input from the switches and output them directly to the LEDs without processor involvement.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    It is not clear exactly what you are trying to implement but I will suggest a couple of options.

     

    You could set up both an 8 bit GPIO input port, connected to the ZedBoard switches, and an 8 bit GPIO output port, connected to the ZedBoard LEDs, and then write 'C' code to read from the 'switches' GPIO port and then write to the 'LEDs' GPIO port. You could do this using either the Zynq PS (Processing System) GPIO or by instantiating AXI GPIO IP blocks in the PL (Programable Logic). In either case the easiest thing to do is let the Vivado tools set the port addresses and use the logical addresses defined. There are a couple of good examples on how to do this using the PS GPIO in two of Adam Taylor's blog entries:

     

    http://forums.xilinx.com/t5/Xcell-Daily-Blog/Using-the-MicroZed-Button-for-Input-Adam-Taylor-s-MicroZed/ba-p/393035

    http://forums.xilinx.com/t5/Xcell-Daily-Blog/Driving-the-Zynq-SoC-s-GPIO-Adam-Taylor-s-MicroZed-Chronicles/ba-p/389611

     

    The other approach would be to design an HDL (VHDL or Verilog) block of logic that would take the input from the switches and output them directly to the LEDs without processor involvement.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    thanks!