Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design How to activate SPI in zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 360 subscribers
  • Views 487 views
  • Users 0 members are here
Related

How to activate SPI in zedboard

ashahsana
ashahsana over 10 years ago

Hello
I am using 7z020 board and I want to receive data from SPI
but the problem is in the /dev folder there is no SPIDEV file .
I did the following steps
In the XPS I design all the hardware , In this particular project I took a simplest case  in which I only add SPI and connected it with EMIO.

This is my constraint file

NET "processing_system7_0_SPI0_MOSI_O_pin" LOC = R19;
NET "processing_system7_0_SPI0_SCLK_I_pin" LOC = D18;
NET "processing_system7_0_SPI0_SS_O_pin" LOC = L21;

NET "processing_system7_0_SPI0_MOSI_O_pin" IOSTANDARD = LVCMOS25;
NET "processing_system7_0_SPI0_SCLK_I_pin" IOSTANDARD = LVCMOS25;
NET "processing_system7_0_SPI0_SS_O_pin" IOSTANDARD = LVCMOS25;

After this step I generate the .bit file and then I made boot file.

after booting the board  problem starts when I didn't find SPIDEV file  in the /dev folder . for this purpose I made devicetree for this particular project using SDK.
and add the following lines
spidev@0{
tcompatible="spidev";
treg =<0>; //chipselect 0
tspi-max-frequency= <50000000>;
t};


and then convert it into .dtb file because it was in .dts.

then rebuild the kernal

when i am using these files the done LED is on but on serial terminal is blank. Blue LEd means my FPGA is programmed and I can see clock means hardware connection is done.

Now where  i am doing mistake can anyone guide me please
May be i am doing mistake here

1. When I rebuild the kernal I put devicetree.dts in the ./ar,/arch/boot/dts folder and .dtb in the ./arch/arm/boot . is it ok???
2.I didn't make my u-boot for this particular program

Can you give me ANY Suggestions
thanks
Sana

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 10 years ago

    Hi Sana,

    Is this for a 7z020 ZedBoard or is it for 7z020 MicroZed, a 7z020 PicoZed target?

    If your serial terminal is blank after creating an entirely new devicetree, I would recommend starting with a known good devicetree and adding the SPI entries to that.

    There is some information for adding SPI support on this wiki page:

    http://www.wiki.xilinx.com/SPI+Zynq+driver

    Make sure you have the top level device entry for the SPI controller added to the devicetree.  If you are using SPI0 you would add the "spi: spi@e0006000" entry.

    Also take a look at this forum entry to make sure that the driver is being built into the kernel correctly.

    https://forums.xilinx.com/t5/Embedded-Linux/Spidev-issue-Spi-transfer-timeout/td-p/548153/page/2

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ashahsana
    0 ashahsana over 10 years ago in reply to zedhed

    Hello
    I have one question ,
    For adding SPIDEV :
    if we change in the devicetree and recompile the kernal then is it enough process for adding the device .
    Do we need some more changes in the kernal??
    thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ashahsana
    0 ashahsana over 10 years ago in reply to zedhed

    Hello
    I have one question ,
    For adding SPIDEV :
    if we change in the devicetree and recompile the kernal then is it enough process for adding the device .
    Do we need some more changes in the kernal??
    thanks