Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design transferring data from PS to PL on LINUX Platfrom
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 359 subscribers
  • Views 1090 views
  • Users 0 members are here
Related

transferring data from PS to PL on LINUX Platfrom

shivangi_29
shivangi_29 over 8 years ago

Hello everyone,

 

I am working on how to tranfer data from processor to FPGA on LINUX platform. I have created my on IP consisting of AXI Lite and AXI Full, please provide some guidence how to program the register of AXI lite and data transfer mechanism through AXI full on LINUX Platform.

 

Thanks & Regards

Shivangi Jaiswal

  • Sign in to reply
  • Cancel
Parents
  • rembo
    0 rembo over 8 years ago

    I was trying the same, can you explain what your block design consists of?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shivangi_29
    0 shivangi_29 over 8 years ago in reply to rembo

    There is a zynq processor and custom IP, interconnection between there two are through AXI interconnect bridge. I have created devicetree.dtb file. I am also controlling ad9364 agile tranceiver through SPI line by creating SPI as a device by doing some changed in .dtb file.Now next step is to transfer data through AXI. I get to know we can do it by UIO method but dont know how to start. 

    plz provide some solution.

    Thanks & Regards

    Shivangi 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shivangi_29
    0 shivangi_29 over 8 years ago in reply to rembo

    There is a zynq processor and custom IP, interconnection between there two are through AXI interconnect bridge. I have created devicetree.dtb file. I am also controlling ad9364 agile tranceiver through SPI line by creating SPI as a device by doing some changed in .dtb file.Now next step is to transfer data through AXI. I get to know we can do it by UIO method but dont know how to start. 

    plz provide some solution.

    Thanks & Regards

    Shivangi 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shivangi_29
    0 shivangi_29 over 8 years ago in reply to shivangi_29

    I have done some changes in .dtb file and UIO0 has been created in /dev/uio0. There is also two mapping shown in /sys/class/uio/maps/mapo/map1. 

    This is my .dtb file

     
     PL.dts
     
     {
    amba_pl: amba_pl {
    #address-cells = <1>;
    #size-cells = <1>;
    compatible = "simple-bus";
    ranges ;
    mod_ip_0: mod_ip@43c00000 {
    compatible = "dmen-uio";
    reg = <0x43c00000 0x10000 0x7aa00000 0x10000>;
    xlnx,s00-axi-addr-width = <0x4>;
    xlnx,s00-axi-data-width = <0x20>;
    xlnx,s01-axi-addr-width = <0xa>;
    xlnx,s01-axi-aruser-width = <0x1>;
    xlnx,s01-axi-awuser-width = <0x1>;
    xlnx,s01-axi-buser-width = <0x1>;
    xlnx,s01-axi-data-width = <0x20>;
    xlnx,s01-axi-id-width = <0xc>;
    xlnx,s01-axi-ruser-width = <0x1>;
    xlnx,s01-axi-wuser-width = <0x1>;
    };
    };
    };
     
    This is programming I have done respective of virtual and physical address mapping
     
      C coding:
       
       
      ad9361_uio_fd = open(AD9361_UIO_DEV, O_RDWR);
      printf("hi");
      if(ad9361_uio_fd < 1)
      {
      printf("%s: Can't open ad9361_uio device\n\r", __func__);
      return;
      }
       
       
       
      FILE *fp;
      uint32_t mem_size=0x10000;
      uint32_t mem_addr=0x43c00000;
      fp = fopen ("/sys/class/uio/uio0/maps/map0/size","r");
      fscanf(fp,"0x%0x", &mem_size);
      fclose(fp);
      fp = fopen ("/sys/class/uio/uio0/maps/map0/addr","r");
      fscanf(fp,"0x%0x", &mem_addr);
      fclose(fp);
       
       
      FILE *fs;
      uint32_t mem_size_1=0x10000;
      uint32_t mem_addr_1=0x77a00000;
      fs = fopen ("/sys/class/uio/uio0/maps/map1/size","r");
      fscanf(fs,"0x%0x", &mem_size_1);
      fclose(fs);
      fs = fopen ("/sys/class/uio/uio0/maps/map1/addr","r");
      fscanf(fs,"0x%0x", &mem_addr_1);
      fclose(fs);
       
      I am stuck at this point. what will be the next step??
       

    Thanks

    shivangi