Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Custom Peripheral slave register writing issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 367 views
  • Users 0 members are here
Related

Custom Peripheral slave register writing issue

Former Member
Former Member over 10 years ago

I created a custom peripheral which has one slave register. I tried to write to this register and read the data back.
I program the FPGA using Xilinx SDK tool. I use xilinx webpack 14.5.
After I use SDK tool to program the chip, I execute  the software. Everything seems working except things related to the custom peripheral. For example, I can read/write with the UART and I can write to the leds on the board using GPIOs. BUT writing and then reading from the custom peripheral fails. For example, When I read, the read value is rubbish but constant value.

When I create an mcs file for the QSPI flash, then program the flash, restart the board and run it, everything WORKS as expected. Then the issue only happens when I try to execute/run the software from the SDK.

Same issue is repeated when I use interrupts from GPIOs. Interrupts only work when I program the flash then run the board again.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 10 years ago

    I am more familiar with ISE tools than vivado.
    I tried using Vivado but could not execute the software on the device.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    I am more familiar with ISE tools than vivado.
    I tried using Vivado but could not execute the software on the device.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data