Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Current load over 3,3V FMC
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 360 subscribers
  • Views 377 views
  • Users 0 members are here
Related

Current load over 3,3V FMC

Former Member
Former Member over 11 years ago

Hi,

can you tell me the maximum current load of the 3,3V FMC port?

Thank you!

  • Sign in to reply
  • Cancel
  • ctammann
    0 ctammann over 11 years ago

    The total current capacity of the 3.3V rail on ZedBoard is designed to provide 3A, the Vadj rail which also feeds the FMC interface is designed to 2A.  Keep in mind that these supplies also power the Vcco banks of the FPGA which may reduce the total current available to the FMC interface.  The 3.3V regulator is capable of 4A, although the circuit is optimized for 3A.  The inductor used is rated for 6A so it should be ok if you exceed the 3A rating by a small margin.  Typically to be safe I like to design the inductors to have a rating of 2x the max system current.
    Thanks
    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to ctammann

    thats exactly what I want to know.
    Thank you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer