Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Interfacing through SPI with Pmod
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 359 subscribers
  • Views 1512 views
  • Users 0 members are here
Related

Interfacing through SPI with Pmod

Former Member
Former Member over 12 years ago

I am trying to use the Zedboard to interface to a PMOD using JA1 connector and do a simple read/write via SPI. I have no found any simple tutorials for this. Can I get some help?

what I really want to do is do the least amount possible through XPS and just simply constrain my pins on the UCS and do everything else in the ARM C code...

(I also need a simple I2C interface and will post a separate thread for this)

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    1, In XPS enable SPI in the XPS Zynq tab.
    2, Set IO to EMIO.
    3, Under Ports tab select ps7_0 and expand (IO_IF) SPI_0.  And change connected port to external ports.
    4, The SPI ports should be listed under "External Ports," now quits XPS, regenerate top level HDL.  You should see ports listed in top level HDL now.
    5, Constraint pins with UCS.

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago

    1, In XPS enable SPI in the XPS Zynq tab.
    2, Set IO to EMIO.
    3, Under Ports tab select ps7_0 and expand (IO_IF) SPI_0.  And change connected port to external ports.
    4, The SPI ports should be listed under "External Ports," now quits XPS, regenerate top level HDL.  You should see ports listed in top level HDL now.
    5, Constraint pins with UCS.

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    After that witch c code I have to write to send "Hello pSoC" through SPI? XSpiPs_Transfer?

    I am trying to connect a ZedBoard whit PSoC via SPI.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer