Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design PL cyclical memory read without PS intervention
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 324 views
  • Users 0 members are here
Related

PL cyclical memory read without PS intervention

ejubenville
ejubenville over 12 years ago

I'm looking for a way to implement cyclical memory reading inside the Zynq PL without the PS having to be involved.  Is it possible?

Suppose I wanted to create an arbitrary digital waveform generator.  I could conceivably define a multi-megabit data pattern in DDR3 memory, and have that data streamed to my PL through a FIFO for output as 1's and 0's at some fixed rate.  When the end of pattern memory is encountered, I'd want to restart from the beginning of the pattern, repeating endlessly.

I cannot figure out which Xilinx IP cores to stitch together to implement something like this without processor involvement.  For example, if I use the AXI FIFO Memory Mapped IP core, it appears that the processor needs to intervene to push new data into the FIFO.  Processor intervention means that the bitrate of the pattern generator is dependent on the operating system response time to interrupts. 

Is there an approach I can use to get the processor out of the loop, so that the PL can fully control the cyclical transfer of memory to the FIFO?

  • Sign in to reply
  • Cancel
  • ejubenville
    0 ejubenville over 12 years ago

    After studying the DataMover peripheral, I think that gives me exactly what I need.  However, I don't know how to coordinate the memory space between Linux and the DataMover.  The DataMover requires a physical memory address in its command bus, but the addresses in my userland host Linux application are virtual addresses.

    Do I need to write a Linux driver to allocate a block of physically contiguous memory with kmalloc()?  If so, is there a driver or loadable module example out there that I can use as is, or clone and hack?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer