Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design LVDS signal to FMC connector
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 887 views
  • Users 0 members are here
Related

LVDS signal to FMC connector

e14 Contributor
e14 Contributor over 11 years ago

Hi,
before I buy the Zedboard, I want to make sure that I can send LVDS (1.8V) signals to the FMC connector pins instead of LVDS_25(2.5V).

Can I send 1.8V LVDS signals to the FMC Pins?

Thank you very much.

Warm regards,

laurnhill

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The Zynq 7020 Banks 34 and 35, which are connected to the FMC connector on the Zedboard, are 'HR' type I/O and can only be configured as LVDS_25 per the 7 Series Select IO Users Guide: http://www.xilinx.com/support/documentation/user_guides/ug471_7Series_SelectIO.pdf

     

    As suggested in this post on the Xilinx Community Forums you may be able to connect LVDS_18 signals to the LVDS_25 signals on the Zynq via the FMC, but you will need to do your own homework to determine if it works for your application.

    http://forums.xilinx.com/t5/Zynq-All-Programmable-SoC/ZedBoard-Bank-34-and-35-HP-I-O-support-for-LVDS-1-8/m-p/639654

     

     

    -Gary