Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Zedboard Revision D Bug Issues (EMIO related)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 359 subscribers
  • Views 897 views
  • Users 0 members are here
Related

Zedboard Revision D Bug Issues (EMIO related)

e14 Contributor
e14 Contributor over 12 years ago

The revision D zedboard has an issue with the EMIO.

Configure a single PS unit (zed default setting) and connect GPIO through EMIO (1-bit) to the LEDs on the board (LED0 or any others), use the following software to control the GPIO to turn the LED on/off:

///////////////////////////
t    XGpioPs Gpio;
t    XGpioPs_Config*GpioConfigPtr;
t    int xStatus;

t    GpioConfigPtr = XGpioPs_LookupConfig(XPAR_PS7_GPIO_0_DEVICE_ID);
t    if(GpioConfigPtr == NULL)
t      return XST_FAILURE;
t    xStatus=XGpioPs_CfgInitialize(&Gpio,
t    GpioConfigPtr,
t    GpioConfigPtr->BaseAddr);
        if(XST_SUCCESS != xStatus)
          print(" PS GPIO INIT FAILED
r");

ttXGpioPs_SetDirectionPin(&Gpio, 54, 1); // the number of the first EMIO is 54
ttXGpioPs_SetOutputEnablePin(&Gpio, 54, 1);
ttXGpioPs_WritePin(&Gpio, 54, 1);
//////////////////////////////////

On revision D board, it does not work, but on revision C board, it works.

So the problem is that  you can not use any PS interfaces, such as SPI, SDIO, "directly" through EMIO to control peripherals devices. We have try SPI (not the QSPI through axi interface) and the SDIO.

We also found an strange way  to solve this problem:  add an AXI-based IP in the project, such as an AXI-GPIO in the PL part, then you can use the PS  interfaces (not the AXI-based) through the EMIO now.

We have try severl boards and it turns out that it is the board version that make this strange issue.

Hope anyone can give an answer ?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Can you tell us what version of Xilinx development tools you are using?

     

    The main difference between a revision C ZedBoard and a revision D ZedBoard is that the revision C board, which was built before Zynq production silicon was available, has an ES (pre production) Zynq device, while a revision D ZedBoard has a production Zynq device.

     

    If you are using earlier Xilinx tool versions, or generated the design and FSBL with earlier tools, they may not have been updated to deal with the production Zynq silicon. And some tool versions act differently in generating level shifters, etc. as well. This Xilinx Answer Record has some details: http://www.xilinx.com/support/answers/51807.htm

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Can you tell us what version of Xilinx development tools you are using?

     

    The main difference between a revision C ZedBoard and a revision D ZedBoard is that the revision C board, which was built before Zynq production silicon was available, has an ES (pre production) Zynq device, while a revision D ZedBoard has a production Zynq device.

     

    If you are using earlier Xilinx tool versions, or generated the design and FSBL with earlier tools, they may not have been updated to deal with the production Zynq silicon. And some tool versions act differently in generating level shifters, etc. as well. This Xilinx Answer Record has some details: http://www.xilinx.com/support/answers/51807.htm

     

    -Gary