Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Understanding Ethernet on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 362 subscribers
  • Views 7380 views
  • Users 0 members are here
Related

Understanding Ethernet on Zedboard

e14 Contributor
e14 Contributor over 11 years ago

Hi Everyone!



I am  not very experienced with the Zedboard and having a ruff time understanding the infrastructure around the Ethernet functionality on the Zedboard.



I have read the related chapters in the following documents, but so far I was not able to put it all together.



1 Zedboard HW User Guide Version 1.1
2 UG585 (v1.10) February 23, 2015
3 various posts such as:
http://zedboard.org/content/redirecting-peripherals-mio-emio



So, as far as I understand there is a Marvell Ethernet PHY on the Zedboard which is directly connected to the PS's MIO Bank 1(via RGMII). Further more, there are two Ethernet MACs in the Processing System which are also connected to the MIO Bank via RGMII(over a GMII/RGMII adapter). Additionally, these two Ethernet MACs are connected to the Zedboards DDR3 RAM via a DMA Controller.



Question A:
Is that correct? Did I miss something important?



One of my goals is to get Ethernet frames/packets into the PL where I want to build some logic to analyse Headers etc.. (proof of concept / educational work)




Similar to Link 3 I redirected eth0 to EMIO(I am working with Vivado btw) and got a MDIO and a GMII Port added to my Processing System block view.




Question B:
Where exactly are these interfaces(GMII and MDIO) connected to? I think to one of the Ethernet MACs of the PS?!




Question(s) C:
What do I have to do now in order to get Ethernet packets to my custom IP?
Do I have to initialize the Ethernet MAC of the PS using DMA(from one of the arm cores) like described in 2 and get packets from RAM to my IP?
Or is there a way to get packets over the above mentioned GMII?
Or is it possible to get a direct connection to the Marvell PHY?




kind regards and a big thank you in advance!

PS:Sorry for the bad formatting.. I added blank lines but paragraphs are not recognized appropriately 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hey,

    thank you for your time!
    I will work trough the labs in no time ;)

    But I still have a question in advance:

    You said: "You can program the Ethernet MAC and DMA controller to transfer the data to any memory area available. Typically this is in the ZedBoard DDR memory but it could be a custom memory area that you have defined and created in the Zynq PL section. Most likely you will want to just move the data from the DDR to your custom IP."


    So, in order to configure the MAC, I have to write data to it's configuration registers which are connected to the axi peripheral bus. Is there a way to access this bus from within the PL or do I have to use the arm core to initialize the MAC etc.. whether I use PL logic to process data or the arm core.

    best regards!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hey,

    thank you for your time!
    I will work trough the labs in no time ;)

    But I still have a question in advance:

    You said: "You can program the Ethernet MAC and DMA controller to transfer the data to any memory area available. Typically this is in the ZedBoard DDR memory but it could be a custom memory area that you have defined and created in the Zynq PL section. Most likely you will want to just move the data from the DDR to your custom IP."


    So, in order to configure the MAC, I have to write data to it's configuration registers which are connected to the axi peripheral bus. Is there a way to access this bus from within the PL or do I have to use the arm core to initialize the MAC etc.. whether I use PL logic to process data or the arm core.

    best regards!