Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design ZED-bare metal SD card write-using drivers-debugging
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 360 subscribers
  • Views 957 views
  • Users 0 members are here
Related

ZED-bare metal SD card write-using drivers-debugging

Former Member
Former Member over 11 years ago

Folks really need your help with this,


Basically I am attempting to write to a 16 GB sandisk microSD card. following the instructions in this link


http://zedboard.org/content/standalone-sd-card-sdio


Here's a brief of the setup:

h/w:
1) 16GB uSD (San disk), fat32 formatted, default allocation size. Zedboard


2) Vivado:
- zynqPS with SD0 and UART1 enabled. MIO 46-CD, 47-WP, and 38( power) is this necessary?, 'Fast speed' and pullups disabled (ON ALL PINS).


-None of the jumpers on my zedboard are set to boot from SD (i.e. J6 or JP7-JP11).


s/w:


Using Yaro's(from the link) C files with the xsdps drivers that it calls.


Here's my debug attempt so far- I basically stepped through the code and a status failure shows up from:


" XSdps_Get_BusWidth() "


stepping into this code I find that, an error flag is actually set in here:


if (StatusReg & XSDPS_INTR_ERR_MASK) {.....


StatusReg is being set just above this if() statement by reading from the XSDPS_NORM_INTR_STS_OFFSET and is being compared with XSDPS_INTR_ERR_MASK (x8000).

I'm wondering if the BlkCnt of 1 that is passed to the address XSdPs_BLK_SIZE_OFFSET is a problem. Because before this it's always been a value of 0.

.....


Thats about as far as I could get before really being at the end of understanding whats going on and how to fix it.


Please..any directions on how to further debug would be HUGELY appreciated.

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 11 years ago

    Hi omkarpradhan,

    I don't think that using debug mode should impact what you are trying to do.

    What version of tools are you using?

    Take a look at this thread here:

    http://microzed.org/content/read-txt-matrices-sd-ddr-zedboard

    In that thread, the XILFFS was used to access the SD card.  On my end, I was at least able to use 2014.4 to build a design where I could run the example code for the XILFFS library on ZedBoard which reads and writes to the SD card.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 11 years ago

    Hi omkarpradhan,

    I don't think that using debug mode should impact what you are trying to do.

    What version of tools are you using?

    Take a look at this thread here:

    http://microzed.org/content/read-txt-matrices-sd-ddr-zedboard

    In that thread, the XILFFS was used to access the SD card.  On my end, I was at least able to use 2014.4 to build a design where I could run the example code for the XILFFS library on ZedBoard which reads and writes to the SD card.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to zedhed

    Kevin,

    Like the title says I am using 2014.2 Are you sure the version difference causes some changes?

    I noted in the link that I had referenced there was something about disabling data chaches. Any idea how to do this?

    Also does my h/w config look correct? Do you have the same setup?

    Omkar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to zedhed

    Holy ***, it works now. Man thanks for that tip about the example.

    Also don't know if changing the h/w config a bit did it. I'm going to run around the block celebrate and then come back to figure the rest of it out.

    I was using a very similar code in another discussion on this forum.

    By the way have you been able to read/write text files? If so any experiments with how fast you can read write?

    Omkar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to zedhed

    Kevin,

    It seems like the default example is set up to write NOT in English. I can't understand the language that it is writing in. I looks to be a mix of chinese/korean script.

    Can you tell me where to change this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer