Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design ZED-bare metal SD card write-using drivers-debugging
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 360 subscribers
  • Views 957 views
  • Users 0 members are here
Related

ZED-bare metal SD card write-using drivers-debugging

Former Member
Former Member over 11 years ago

Folks really need your help with this,


Basically I am attempting to write to a 16 GB sandisk microSD card. following the instructions in this link


http://zedboard.org/content/standalone-sd-card-sdio


Here's a brief of the setup:

h/w:
1) 16GB uSD (San disk), fat32 formatted, default allocation size. Zedboard


2) Vivado:
- zynqPS with SD0 and UART1 enabled. MIO 46-CD, 47-WP, and 38( power) is this necessary?, 'Fast speed' and pullups disabled (ON ALL PINS).


-None of the jumpers on my zedboard are set to boot from SD (i.e. J6 or JP7-JP11).


s/w:


Using Yaro's(from the link) C files with the xsdps drivers that it calls.


Here's my debug attempt so far- I basically stepped through the code and a status failure shows up from:


" XSdps_Get_BusWidth() "


stepping into this code I find that, an error flag is actually set in here:


if (StatusReg & XSDPS_INTR_ERR_MASK) {.....


StatusReg is being set just above this if() statement by reading from the XSDPS_NORM_INTR_STS_OFFSET and is being compared with XSDPS_INTR_ERR_MASK (x8000).

I'm wondering if the BlkCnt of 1 that is passed to the address XSdPs_BLK_SIZE_OFFSET is a problem. Because before this it's always been a value of 0.

.....


Thats about as far as I could get before really being at the end of understanding whats going on and how to fix it.


Please..any directions on how to further debug would be HUGELY appreciated.

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 11 years ago

    Hi Omkar,

    I am not sure that the xilffs_polled_example.c is setup to write in any specific language.

    If I look inside of FfsSdPolledExample() for SDK 2014.4, I can see the following test pattern get setup within a buffer:

    #define TEST 7

    ...

    for(BuffCnt = 0; BuffCnt < FileSize; BuffCnt++){
       SourceAddress[BuffCnt] = TEST + BuffCnt;
    }

    That ends up being a bunch of sequential 32-bit word data so it just so happens when you open the file it appears to be NOT in English.  If you open the file with a HEX editor, you should see a data pattern starting at 0x00000007 and counting upward from there.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 11 years ago

    Hi Omkar,

    I am not sure that the xilffs_polled_example.c is setup to write in any specific language.

    If I look inside of FfsSdPolledExample() for SDK 2014.4, I can see the following test pattern get setup within a buffer:

    #define TEST 7

    ...

    for(BuffCnt = 0; BuffCnt < FileSize; BuffCnt++){
       SourceAddress[BuffCnt] = TEST + BuffCnt;
    }

    That ends up being a bunch of sequential 32-bit word data so it just so happens when you open the file it appears to be NOT in English.  If you open the file with a HEX editor, you should see a data pattern starting at 0x00000007 and counting upward from there.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data