Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design DPR on Zedboard under Yocto Linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 359 subscribers
  • Views 195 views
  • Users 0 members are here
Related

DPR on Zedboard under Yocto Linux

100aditya
100aditya over 9 years ago

Hi Sir,

         I have done till now:-

1- I am able to boot the Yocto linux on the Zedboard.
2- I have intergrtaed the Texas wifi module (WL1835MODCOM8) with the Pmod avialble on the ZedBoard.
3-  After this i connected one PC and this prepared Zedboard(in above two steps) on my local wireless LAN.
4-  From the PC, i can Ping the ZedBoard in my wireless network
5-  On this i ran the tftp server on PC and  I sent some file of upto 1 Mb to this Zedboard using wireless Media.
 
    Now suppose that PL part of the Zedboard is configured with some logic(let us assume the logic is UP Counter). Now i want to send one file(partial reconfiguartion file:- Down Counter logic) from PC to  this Zedboard(on which Yocto Linux is running). Once this file is reached to this Zedboard i want this file(partial reconfiguartion file) to change the UP Counter logic to Down Counter Logic.
 
     I want DPR to be done from the Yocto Linux which is running on the Zedboard.
     Basically I have one one Zedboard on which Yocto Linux is running. Now there is some reconfig logic in the PL on this Zedboard.Now i want to change this reconfig logic. So for this i have to send the DPR bit stream to the ZedBoard and once this is reached to the Zedboard, after that this DPR file should reconfigure the PL portion.
 
    I have tried to write what is task that i want to achieve.
 
Please provide me some details/references to execute my above task.
 
Regards
Aditya