Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Send data from the PL to UART0
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 359 subscribers
  • Views 391 views
  • Users 0 members are here
Related

Send data from the PL to UART0

e14 Contributor
e14 Contributor over 12 years ago

Hi guys,

I've seen this in many questions here but couldn't get my answer. I just want to create a very simple design to understand how I can interact with the UART from the PL.
What I have done so far is to add a AXI UART Lite to the PL. I just want to see how I can connect the ports from this to the UART0 and send just receive a data from the UART0 and send it back to the console.


Thanks a lot

  • Sign in to reply
  • Cancel
Parents
  • metinburak_
    0 metinburak_ over 12 years ago

    When you create the AXI UART Lite in PL, it's connected to the PS via the M_AXI_GP0, which means the PS is master and the UART Lite is slave. The slave UART module's line ports are routed to the external pins, and the control interface is connected to the PS as being an AXI slave. No alternative routing is allowed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • metinburak_
    0 metinburak_ over 12 years ago

    When you create the AXI UART Lite in PL, it's connected to the PS via the M_AXI_GP0, which means the PS is master and the UART Lite is slave. The slave UART module's line ports are routed to the external pins, and the control interface is connected to the PS as being an AXI slave. No alternative routing is allowed.