Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Standalone System In Zedboard and FMCOMMS2
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 362 subscribers
  • Views 848 views
  • Users 0 members are here
Related

Standalone System In Zedboard and FMCOMMS2

e14 Contributor
e14 Contributor over 9 years ago

Good afternoon everyone,

 
   I am working on a project to connect the Zedboard and FMCOMMS2 using the HDL workflow advisor.
 
    
 
   What I want to do is to have the Zynq FPGA (PL, not the processor) generate samples of a sine wave and send these to the RF for transmission FMCOMMS2, and to have this system operating stand-alone, without any further connection to the PC running Simulink.
 
    
  It seems to me that, the way I have the project set up, I need to keep Simulink connected to the board, even if it is not doing any processing. If I disconnect the ZedBoard from the PC, I get an error message on the PC. By "disconnect", I mean literally unplugging the Ethernet cable from the PC's port. The error message specifies that "a runtime error occurred in the System Object 'comm.internal.SDRTxZedBoardFMC234SL', while executing the 'stepImpl' method" .
   
  I would also like to know if it's possible to save the generated bitstream into a bootable image, so that I whenever I turn the board on, I get the desired functionality. I have followed the instructions in the PicoZed SDR SpeedWay 2015 Training but it doesn' work. I
   

I have attached a Word document with more details about how I have my project set up; also, the project folder with all the files. I'd be grateful if you could take a look at it and see if I'm doing everything correctly.
   

Word document: https://www.sendspace.com/file/ygi7ed

 

Project files: https://www.sendspace.com/file/41580t.  

 

Thanks for your help,

Romel

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Hi Matt,

     

    Just to clarify, when I said "I am not very confident about the "devicetree.dtb", and "uImage" ".  I believe that I should modify something on them  to run my new project.

     

    Thanks,

     

     Romel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Hi Matt,

     

    Just to clarify, when I said "I am not very confident about the "devicetree.dtb", and "uImage" ".  I believe that I should modify something on them  to run my new project.

     

    Thanks,

     

     Romel