Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Blink a LED only with Zynq FPGA(without using SDK)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 359 subscribers
  • Views 4343 views
  • Users 0 members are here
Related

Blink a LED only with Zynq FPGA(without using SDK)

e14 Contributor
e14 Contributor over 10 years ago

Hello,
I've followed the tutorials of section 1 and 4 in the Zynq Book Tutorials, they explained how to do a basic design on the ZedBoard and how to create an IP. The result of both tutorials was a LED that was blinking. However, both examples used the SDK and so the CPU of the ZedBoard.

I want to be able to design circuits only on the Zynq FPGA(without using the ARM processor). Can you please give me a tutorial/step by step explanation of how can I blink a LED on the ZedBoard when pressing a button by using only the CPU? I am using Vivado Web Edition, version 15.4.

Thank you!

PS:The VHDL code to do this would look like:
ENTITY part1 IS
PORT ( SW : IN STD_LOGIC_VECTOR(9 DOWNTO 0);
LEDG : OUT STD_LOGIC_VECTOR(9 DOWNTO 0)); - - green LEDs
END part1;
ARCHITECTURE Behavior OF part1 IS
BEGIN
LEDG <= SW;
END Behavior
However, at which stage in Vivado should I do the pin assignation for example?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Unless you want to use the JTAG interface to load your bitstream you will need at least a minimal Zynq PS block in your design to load the bitstream from the SD Card or QSPI Flash. There are quite a few tutorials on how to do this.

     

    The simplest are probably the MicroZed Tutorials, which should work for you if you just target the ZedBoard:

     

    http://zedboard.org/support/design/1519/10

     

    But it sounds like you could really benefit from a more complete training. Both the Zynq Software and Hardware Speedway workshops target the ZedBoard (or the MicroZed) and offer a much more in depth look at how the Zynq device and tools work:

     

    http://zedboard.org/support/trainings-and-videos

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Unless you want to use the JTAG interface to load your bitstream you will need at least a minimal Zynq PS block in your design to load the bitstream from the SD Card or QSPI Flash. There are quite a few tutorials on how to do this.

     

    The simplest are probably the MicroZed Tutorials, which should work for you if you just target the ZedBoard:

     

    http://zedboard.org/support/design/1519/10

     

    But it sounds like you could really benefit from a more complete training. Both the Zynq Software and Hardware Speedway workshops target the ZedBoard (or the MicroZed) and offer a much more in depth look at how the Zynq device and tools work:

     

    http://zedboard.org/support/trainings-and-videos

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hello Gary,
    Thank you for your answer.
    Can you please tell me which tutorial exactly shows how can I program the FPGA without using the SDK. I looked at the links and they all seem to be using the ARM CPU.