Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design Blink a LED only with Zynq FPGA(without using SDK)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 359 subscribers
  • Views 4346 views
  • Users 0 members are here
Related

Blink a LED only with Zynq FPGA(without using SDK)

e14 Contributor
e14 Contributor over 10 years ago

Hello,
I've followed the tutorials of section 1 and 4 in the Zynq Book Tutorials, they explained how to do a basic design on the ZedBoard and how to create an IP. The result of both tutorials was a LED that was blinking. However, both examples used the SDK and so the CPU of the ZedBoard.

I want to be able to design circuits only on the Zynq FPGA(without using the ARM processor). Can you please give me a tutorial/step by step explanation of how can I blink a LED on the ZedBoard when pressing a button by using only the CPU? I am using Vivado Web Edition, version 15.4.

Thank you!

PS:The VHDL code to do this would look like:
ENTITY part1 IS
PORT ( SW : IN STD_LOGIC_VECTOR(9 DOWNTO 0);
LEDG : OUT STD_LOGIC_VECTOR(9 DOWNTO 0)); - - green LEDs
END part1;
ARCHITECTURE Behavior OF part1 IS
BEGIN
LEDG <= SW;
END Behavior
However, at which stage in Vivado should I do the pin assignation for example?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    If you would like to upload the bit-file (part1.bit) created by the script above you can save the following into program.tcl


    open_hw
    connect_hw_server -url TCP:localhost:3121
    set hw_target [get_hw_targets */xilinx_tcf/*]
    current_hw_target $hw_target
    set_property PARAM.FREQUENCY 6000000 $hw_target
    open_hw_target
    set fpga [lindex [get_hw_devices] 1]
    set_property PROGRAM.FILE part1.bit $fpga
    program_hw_devices $fpga
    exit

    Assuming the USB JTAG cable is connected to your Zedboard you should be able to load the bitfile using:

    vivado -mode tcl -source program.tcl

    After it has completed you should be able to flip the switches and watch the LED's change.

    If you have successfully done this you know that your hardware and toolchain is working correctly. Then you should try to go for some tutorials and other training.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    If you would like to upload the bit-file (part1.bit) created by the script above you can save the following into program.tcl


    open_hw
    connect_hw_server -url TCP:localhost:3121
    set hw_target [get_hw_targets */xilinx_tcf/*]
    current_hw_target $hw_target
    set_property PARAM.FREQUENCY 6000000 $hw_target
    open_hw_target
    set fpga [lindex [get_hw_devices] 1]
    set_property PROGRAM.FILE part1.bit $fpga
    program_hw_devices $fpga
    exit

    Assuming the USB JTAG cable is connected to your Zedboard you should be able to load the bitfile using:

    vivado -mode tcl -source program.tcl

    After it has completed you should be able to flip the switches and watch the LED's change.

    If you have successfully done this you know that your hardware and toolchain is working correctly. Then you should try to go for some tutorials and other training.