Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
ZedBoard Hardware Design ZedBoard CTT Booting Linux from the SD Card Problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 359 subscribers
  • Views 345 views
  • Users 0 members are here
Related

ZedBoard CTT Booting Linux from the SD Card Problem

Former Member
Former Member over 11 years ago

I am attempting the "Take a Test Drive" in chapter 5.2.7 of the ZedBoard CTT with Vivado 2013.4.  I having the following files from the ZIP file that came with the download to the FAT32 formatted SD card:
-
-
boot.bin
devicetree.dtb
ramdisk8m.image.gz
zimage

-
-
When I boot the ZedBoard I get the following:
-
-
--------------------------------------------------------------

U-Boot 2011.03-00226-gd4000b9 (Jun 07 2012 - 18:04:19)



DRAM:  512 MiB
MMC:   SDHCI: 0
Using default environment



In:    serial
Out:   serial
Err:   serial
Net:   zynq_gem
Hit any key to stop autoboot:  0
Copying Linux from SD to RAM...
Unknown command
Device: SDHCI
Manufacturer ID: 27
OEM: 5048
Name: SD04G
Tran Speed: 25000000
Rd Block Len: 512
SD version 1.10
High Capacity: Yes
Capacity: 3980394496
Bus Width: 1-bit
reading zImage



** Unable to read "zImage" from mmc 0:1 **
reading devicetree.dtb



** Unable to read "devicetree.dtb" from mmc 0:1 **
reading ramdisk8M.image.gz



** Unable to read "ramdisk8M.image.gz" from mmc 0:1 **
## Starting application at 0x00008000 ...


---------------------------------------------------------------
-

I've also tried following the instructions in 5.2.5 to generate boot.bin from in SDK using the zynq_fsbl_0.elf and u-boot.elf, but I get the same results.
-
-
Btw, the formatting recognition suck and is not adding line breaks or paragraphs automatically, as it says it will.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    Reformatting the SD Card fixed the problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago

    Reformatting the SD Card fixed the problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data